STM32 MCUs
From FAQs to complete How-to articles, find useful articles on STM32 MCUs programming, troubleshooting, ecosystem, and product details.
cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge base articles

How to use function pointers in STM32CubeIDE

Summary This article provides a step-by-step guide and example regarding how a function pointer is implemented and used. The basic usage and a simple example application are provided using the NUCLEO-G071RB board but can be easily tailored to any ot...

BMontanari_0-1730142065473.png BMontanari_1-1730142065475.png

How to select suitable endpoints for your STM32 USB application

Introduction The article provides a comprehensive guide on selecting suitable endpoints for USB applications using STM32 microcontrollers. This involves understanding the types of data transfers required by the application and determining suitable en...

FBL_0-1729619247624.png FBL_1-1729624203582.png
FBL by ST Employee
  • 6041 Views
  • 0 comments
  • 2 kudos

Configuring DSP libraries on STM32CubeIDE

This FAQ concerns the DSP Libraries, how to integrate them in an STM32CubeIDE project and to execute an example based on the Digital Signal Processing. Note: If you are using CMSIS V 5.8.0, refer to the article below. How to integrate CMSIS-DSP libra...

1300.jpg 1301.jpg 1303.jpg 1304.jpg

ADC interleaved mode (2/2): Hands-On STM32CubeIDE project

This series of articles will provide you with: Tips&tricks on how to implement ADC interleaved mode to double equivalent sampling rateADC interleave mode details from practical point of viewInfo on DMA data transfer using ADC Common Data Register Par...

1509.png 1510.png 1511.png 1512.png
LauraCx by ST Employee
  • 11600 Views
  • 2 comments
  • 3 kudos

How to connect to the STM32 CAN Bootloader interface

The bootloader inside STM32 families uses the protocol described in AN3154. It is supported by the STM32F1, F2, F4, F7, L4 series. The purpose of this article is to give a guide on how to connect to a STM32 CAN bootloader Target, to erase and program...

10.jpg 11.png 12.png 13.png

Downloading STM32Cube packages from GitHub correctly

You will receive one or more compilation errors if you download any given STM32Cube package by using the GitHub Download ZIP option.  This is because our repository is created using the git submodule command. So, if the GitHub Download ZIP option is...

STTwo-32 by ST Employee
  • 5498 Views
  • 1 comments
  • 1 kudos

How to change STM32CubeIDE to dark theme

If you want a customized interface to work on your projects, you can try the alternatives offered by the STM32CubeIDE to personalize the appearance of your files. To change the default settings to give it a personal touch, follow the steps below. Cre...

273.png 274.png 275.png 276.png

Overall FAQs for QUADSPI/OCTOSPI/HSPI/XSPI

Introduction The purpose of this article is to provide external memories tips and tricks, frequently asked questions, and a list for useful link resources.  1. Overall FAQs for QUADSPI/OCTOSPI/HSPI/XSPI  1.1 How to check whether a device is supported...

KDJEM.1 by ST Employee
  • 7950 Views
  • 0 comments
  • 2 kudos

IWDG early wakeup interrupt in Stop modes for STM32U5

Introduction  The IWDG (Independent Watchdog) offers the possibility to exit from stop modes in STM32U5. The wakeup from stop with interrupt is supported in Stop 0, Stop 1, Stop 2, and Stop 3 modes for STM32U535/545/59x/5Ax/5Fx/5Gx as described in t...

IWDG in lp modes.PNG PA5 GPIO output.PNG IWDG config.PNG LL config.PNG
Sarra.S by ST Employee
  • 2166 Views
  • 0 comments
  • 1 kudos

How to use the input capture feature

Introduction  Input capture is one of the advanced timer features available on the STM32 microcontrollers. This article guides you through the theoretical aspects of input capture, provide a practical example, and discuss troubleshooting common issu...

clock configuration.png input capture mode.png TIM2 configuration.png TIM2 interrupt.png
Sarra.S by ST Employee
  • 44535 Views
  • 6 comments
  • 5 kudos

FAQ: Using dead battery pins in an STM32 with an integrated UCPD

Introduction Dead battery configuration control (DBCCx) pins play a crucial role in USB Type-C® applications to manage scenarios where the device's main power source is unavailable (dead battery). These pins, used with configuration channel (CC) pin...

FBL_3-1725455948265.png FBL_4-1725455948270.png FBL_5-1725455948294.png
FBL by ST Employee
  • 3257 Views
  • 0 comments
  • 4 kudos

How to integrate the X-CUBE-MEMS1 package with your project

Summary      The article offers an in-depth demonstration of incorporating the X-CUBE-MEMS1 software package into an STM32CubeIDE project, tailored specifically for the B-U585I-IOT02A board with its onboard ISM330DHCX accelerometer. Introduction T...

BMontanari_4-1725298070140.png BMontanari_5-1725298129333.png BMontanari_6-1725298166170.png BMontanari_7-1725298415774.png

How to add external libraries in STM32CubeIDE

Summary This article shows how to integrate a library, in the form of an achieve file (*.a) in your project, so you can use the functions of the library with a simple header file.  Introduction A library can be defined as a set of nonvolatile resour...

BMontanari_0-1705353822184.png BMontanari_1-1705353822195.png BMontanari_2-1705353822203.png BMontanari_3-1705353822221.png