Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC58 Ethernet

Hello!I am studying the SPC58NH92E7. My chose of MCU is driven by the need to have two Fast Ethernet transceivers operating simultaneously.I'm looking for baremetal (no OS) example for 100BASE-TX. Has anyone come across examples like this? I couldn't...

SPC58NN JTAG Lock and Unlock

Hi Team,We have a requirement to lock the JTAG for the SPC58NN controller.Could anyone please share the detailed procedure to:Lock/disable the JTAG debug accessConfigure password-based protectionUnlock/re-enable the JTAG access using the passwordAny ...

SPC58 and SPC5Studio terms

Hello!I am studying the SPC58NH92E7.I'd like to clarify some terms and definitions. Below, I’ll explain how I understand these terms. Please correct me if I’m wrong.Project examples in SPC5Studio are divided into two classes: "RLA" and "cut2_RLA".RLA...

DEBUG IDE TOOLS FOR SPC582B

For SPC582B, which development IDE is recommeded for code debug and run? Does PLS JTAG debugger software ok to run some demo when using SPC582B-DIS discovery board?

db16122 by Associate II
  • 162 Views
  • 1 replies
  • 0 kudos

Stellar SR5E1 HAL driver

Are HAL drivers and/or LL driver available for SR5E1E3 or E1E5?Where can be found?I saw some HAL LL drivers fin the MCTK SR5E1x Motor Control Toolkit 1.3.0 folder in Stellar Studio (\StellarStudio-9.0\contrib\SR5E1_MCTK-1.3.0\) but they are not prese...