Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Firmware Update for F446 and ST67

[Part Numbers] NUCLEO-F446RE, ST67W611M1[Environment] STM32CubeIDE Version 2.1.1, ST67 Firmware Version V1.3.0[Details]Currently, the FOTA code generated by STM32CubeMX can only update the ST67 firmware; the F446 firmware cannot be updated.Furthermor...

Jerrylin00_1-1780302225560.png Jerrylin00_0-1780302117116.png

Resolved! ST4SIM-300M Getting the same ICCID

Hi! We have two custom boards that we have soldered the ST4SIM-300M eSim to. We have earlier been using the ST4SIM-200M and followed this activiation procedure:https://www.st.com/resource/en/application_note/an5740-st4sim-with-truphone-connectivity--...

mackzswe by Associate
  • 623 Views
  • 6 replies
  • 2 kudos

S2-LP with ASK

I'm trying to configure the S2-LP with the following settings:- Base frequency: 915 Mhz;- Modulation: ASK (modulation depth 90%, '1'=10dBm and '0'=0dBm);- Data rate: 80kbps;- Channel space: 389kHz;- Channel: 0. I've developed a HAL because using the ...

Measurement.png
pzt by Associate III
  • 88 Views
  • 1 replies
  • 0 kudos

STUSB4531 PPS SUPPORT

Hi all,I was super exited to test the new STUSB4531 IC on the EVAL-SCS006V1.The PPS support of the chip is the main reason to pass over from the STUSB4500. I have done a lot of test with 100W PPS enabled USB-C supply but without luck. i did not manag...

STUSB4531-18V.png
KPTD by Associate
  • 359 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.