STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1835 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4989 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9742 Views
  • 5 replies
  • 3 kudos

No access to GPIO on EVB EVALSPIN32G0A1

HiI would like to generate a PWM signal on a pin on the board of the EVALSPIN32G0A1 EVB, but no signal is being generated. I tried doing it onthe pins of J5 (the hall conctors pins) and on the pins of J2 but no ignal is generated there. i tried check...

Ofer by Senior
  • 33 Views
  • 0 replies
  • 0 kudos

failed to start GDB server

Hello everyone,I am facing a flashing/debugging issue with the STEVAL-SPIN3202 Rev 3.1 board.Board:STEVAL-SPIN3202 Rev 3.1Software Used:STM32CubeIDESTM32CubeProgrammerProblem:While trying to flash or debug the board from STM32CubeIDE, I get the follo...

stm32g474 hrtim seting for vfd

Hello ST Support Team,I am working on an STM32G474RE based 3-phase VFD using HRTIM1 for SVPWM generation.Hardware/output:- Timer A/B/C used for U/V/W phases- TA1/TA2, TB1/TB2, TC1/TC2 complementary PWM- Dead-time enabled- Center-aligned PWM required-...

REALIZE by Associate
  • 48 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.