on 2024-10-22 6:00 AM - edited on 2025-11-28 7:39 AM by Amel NASRI
This article dives into how you can avoid communication disruptions. In some cases, you may see that FDCAN messages are repeated even though they’re acknowledged. You may also observe some other unexpected behavior. We cover a possible cause of the issue and how to solve it.
When a communication issue appears, a possible cause can be the noncompliance to the following rule shown below.
The FDCAN requires that the CAN time quanta clock is always below the APB clock.
|
|
fdcan_tq_ck < fdcan_pclk |
|
Two clocks are applied to the FDCAN peripheral as shown on the following table extract from the reference manual of STM32H5 (RM0481).
The kernel clock directs to the FDCAN core, which manages the CAN protocol, the communication lines, and the baud rate.
The APB clock allows configuration and control of the FDCAN subsystem through registers, and also to access the message RAM.
|
STM32N6, STM32H7 |
STM32L5, STM32U3, STM32U5, STM32C092, STM32G0, STM32G4, STM32H5, STM32H7RS |
|---|---|
The two block diagrams above are extracts respectively of the reference manual of STM32H72x/3x (RM0468) and of the reference manual of the STM32G4 (RM0440).
They display both 3 FDCAN units and a common block on the top. The clock domains, APB and kernel, are displayed with different colors: light and dark gray, or light yellow and gray.
The FDCAN peripheral is connected to the APB1 peripheral bus (refer to the MCU block diagram in the datasheet, generally figure 1). In STM32CubeMX, the FDCAN peripheral clock fdcan_pclk is the APB1 peripheral bus clock as shown in the image below.
The kernel clock fdcan_ker_ck is delivered through a multiplexer allowing to choose among several sources.
The FDCAN cores are clocked by a common FDCAN time quanta clock fdcan_tq_ck that is used to define the baud rate of the communication channel.
As shown on the block diagram, this clock is generated from the kernel clock as follows:
fdcan_tq-ck = fdcan_ker_ck / DIV
Depending on the STM32 series, the divider is defined by the CDIV[0..3] bits in the FDCAN_CCU_CCFG register (STM32H7) or by the PDIV[0..3] bits in the FDCAN_CKDIV register (for other STM32 series).
The value by default is DIV = 1. When necessary, the divider can be modified to comply with the rule given above between the time quanta clock and the APB clock (fdcan_tq_ck < fdcan_pclk).
The table below summarizes the conditions applying to DIV.
|
|
||||||||||||
The FDCAN requires that the CAN time quanta clock is always below the APB clock.
|
|
fdcan_tq_ck < fdcan_pclk |
|
When necessary, a divider is applied between the kernel clock and the time quanta clock to comply with this rule.
fdcan_tq-ck = fdcan_ker_ck / DIV
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.