MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSM gyroscope scale factor error

I have been analyzing the behavior of the gyroscope thoroughly in order to quantify its drift. I did this by mounting the LSM6DSM onto a step motor and measuring its output. I tried this for two different devices which gave me for one device a consta...

Resolved! SSC Driver support LSM6DSV for QCS8550 board

Hello Team,We are using Qulacomm board QCS8550 Aikri kit with LE r90 release for production, In that there is SSC driver support of LSM6DSV Our setup includes two LSM6DSVTR IMU sensors, and we are attempting to read and write sensor data over SSC usi...

Sensor Tile Box Pro - Evaluation comment

 This is a comment it is not a question.  The older the mems sensor in acceleration the more likely it was to have a thermal effect below 1 Hz.  On the old CX1 from Sensr it was pronounced on three axes, on the MKI109 -210 combination it was reduced,...

Smithson_0-1780756773254.png

LSM6DSM: fifo timestamp drift regularly

LSM6DSM setting: acc/gyro/fifo ODR 208hz, timer resolution 25us, FIFO continous mode# 1. Enable Block Data Update (BDU) and Auto-increment (IF_INC) imu.__write_reg(CTRL3_C, 0x44) # 2. Timestamp resolution (25 us / LSB) # TIMER_HR (bit 5) = 1 in WAKE...

chobits by Associate
  • 47 Views
  • 0 replies
  • 0 kudos

LIS3DSH working wakeUp example

Hello after some headaches with the issue of getting wakeup interrupt working in LIS3DSH accelerometer. I got a working configuration, i would like to share with other users.This example generate a INT1 pulse (50us) each time LIS3DSH is moved. Note a...

LPS27HHTW in SPI mode

If the LPS27 pressure sensor works fine under I2C, I cannot make it repond through the SPI bus.The SPI interface is setup as 4-wire Motorola format (phase 1 polarity 1). CS, the clock SCP and SDI are driven from the SPI controller; SDO is connected t...

mdbot by Associate
  • 86 Views
  • 4 replies
  • 0 kudos

LSM6DSV temperature sensitivities ?

im developing VRtracker using the LSM6DSV recently,and im little bit concerned about the yaw motion stability。especially g-sensitivitydoes it effects apparently?or does it have a specific value?and also does the thermal drift of the internal RC oscil...

Resolved! ROHS Certificate for FXLS8974CFR3

HI Request you to kindly share the RoHS certificate for FXLS8974CFR3 on priority, as it is required urgently.Appreciate your quick support on thisREgardsRaguraman J 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.