Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

solar battery charger

hello, I am using the STEVAL-ISV012V1 demonstration board, which is based on the SPV1040 solar voltage boost converter and the L6924D single-cell Li-ion battery charger.My solar panel consists of 4 parallel solar cells. The solar cell is: KXOB201K04T...

rapr1ext_2-1780862692747.png rapr1ext_0-1780861971668.png rapr1ext_1-1780862061004.png

Resolved! VNF9Q20F VCC pin

For the VNF9Q20F, the datasheet states that the exposed thermal pad (TAB) is VCC.Can someone confirm that the large exposed pad on the bottom of the package is electrically connected to VBAT/VCC and not GND?If so, should the thermal pad and all therm...

Snipaste_2026-06-06_15-58-21.png
qiurui by Associate
  • 51 Views
  • 2 replies
  • 0 kudos

VN9D30Q100 PWM control

Dear sir:I was used VN9D30Q100FTR 6-channel high-side driver for automotive electronic products,the schematic diagram below: According to the datasheet, the PWM clock should be provided via the PWM_CLK input, but there was also this note about the P...

zhi_sai_0-1780541107400.png
zhi_sai by Associate
  • 54 Views
  • 1 replies
  • 0 kudos

L9779WDAT2 compatibility

Hi, i need to replace a L9779WDAT2, it seems that only the WD-SPI version is avaiable.  are thoses two retro compatible, i cannot find data sheet for the WDAT2 anywhere. thanks.

Resolved! Can't configure the TCPP01-M12 to 2.5W (500mA)

Hi,I have follow the DS12900 Rev 7 Figure 21 (Schematic example for USB Type-C at 2.5W with TCPP01-M12) and still can draw more that 1.5A from USB PD source, the voltage seen on CC1 is close to 1.4V (which corresponds to 3A capability). Not sure what...

POLessard_0-1780418199847.png

Resolved! L9369: SPI interface questions

Hi, Good day, May we seek your expertise for the following inquiry: 1. What is the SPI frame format for L9369 RT?2. Is it configurable via SPI?3. What is the default SPI frame configuration for L9369 RT? Thank you.

FTCGIE by Associate
  • 212 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.