STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SIL Rating

I have a question regarding the use of STM32F4 devices in IEC 61508 SIL2/SIL3 applications. The STM32 Safety Library documentation indicates that STM32 devices can be used in SIL2/SIL3 applications. However, I could not find an explicit Hardware Syst...

Him_ by Associate
  • 107 Views
  • 4 replies
  • 1 kudos

Debugging with STM32U3 and OEMiRoT_Appli_TrustZone

Hi ST,I can't seem to get debugging to function when following the above named example on a nucleo-u385RG-Q using CubeIDE and CubeProgrammer. The guidance on the README is vague when it needs to be clear - for starters what is the 'offset of the firm...

AdsBot by Associate II
  • 83 Views
  • 3 replies
  • 1 kudos

Option bytes are not programmed during SFI

Hello,STM32H533 It seems that Option Bytes are not programmed during SFI ??To keep things simple, I changed BOR_LEV, but after SFI, the BOR_LEV was not programmed.Also, I would like to move product state to closed (0x72), that that is also not progra...

lp242 by Associate
  • 50 Views
  • 0 replies
  • 0 kudos

attestation roots for stm32 U3C5

Hi, I have a NUCLEO-U3C5ZI-Q board, and I'm trying to follow the DUA_USER attestation process.   I noticed that the existing Root CA certificates like here https://github.com/STMicroelectronics/STM32CubeU3/blob/main/Utilities/Certificates/ do not ver...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.