STM32 MCUs
From FAQs to complete How-to articles, find useful articles on STM32 MCUs programming, troubleshooting, ecosystem, and product details.
cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge base articles

How to run a CoreMark® benchmark on an STM32

Introduction This article guides you on how to perform CoreMark® benchmarks on an STM32H5 microcontroller. For this article, we use a NUCLEO-H563ZI board, which has an STM32H563ZIT6 MCU that integrates an Arm® Cortex® M33 CPU. This code can be easily...

Lionking_0-1722899611311.jpeg Lionking_1-1722899690190.png Lionking_2-1722899690202.png Lionking_4-1722899690217.png
Lionking by ST Employee
  • 6722 Views
  • 0 comments
  • 1 kudos

How to run a Dhrystone/DMIPS benchmark on an STM32

Introduction This article guides you on how to perform Dhrystone tests on an STM32L5 microcontroller. For this article, we use a NUCLEO-L552ZE-Q board, which has an STM32L552ZET6QU MCU that integrates an Arm® Cortex® M33 CPU. This code can be easily ...

Lionking_0-1722898420188.jpeg Lionking_1-1722898420198.png Lionking_2-1722898420209.png Lionking_3-1722898420221.png
Lionking by ST Employee
  • 7765 Views
  • 0 comments
  • 1 kudos

How to conduct a STM32 self-schematic review PT. 2

In this two-part article we will cover several main areas of focus when conducting a self-review of a custom STM32 schematic and share some hardware debugging tips.If you haven’t yet reviewed the first part of this article, we highly encourage you to...

995.png 996.png 998.png 1000.png

How to set USB CDC line coding

1. What is line coding? Line coding is used to transfer parameters of UART interface, which is emulated using USB CDC - Virtual COM port. In STM32 legacy USB library line coding is handled by a function called CDC_Control_xS (FS for Full speed USB mo...

DMA is not working on STM32H7 devices

The problem is related to two things: memory layout on STM32H7 and internal data cache (D-Cache) of the Cortex-M7 core.  In summary these can be the possible issues: Memory placed in DTCM RAM for D1/D2 peripherals. Unfortunately, this memory is used ...

698.png 700.png Laurids_PETERSEN_0-1690194613355.png 701.png

Debugging in external memory on STM32CubeIDE

Introduction This article describes how to debug in external memory on STM32CubeIDE based on the example provided in the following GitHub repository: STM32CubeH7/Projects/STM32H7B3I-EVAL/Applications/ExtMem_CodeExecution.Regarding hardware, we use th...

Pape_0-1722844618104.png code change.png Pape_2-1722845880991.png Pape_3-1722845895581.png

ADC value affected by ETH PHY 50 MHz from RMII interface

Ethernet reference clock affecting ADC values in STM32 microcontrollers In various STM32 microcontroller applications, the Ethernet reference clock (ETH_REF_CLK) has been observed to introduce noise into ADC (analog-to-digital converter) measurements...

STea_0-1720793800459.png STea_1-1720793848676.png
STea by ST Employee
  • 3318 Views
  • 1 comments
  • 2 kudos

Handling multiple TCP clients on STM32H563 with NetX Duo

Summary In this article, we guide the users of the Azure NetX Duo middleware to handle multiple TCP clients on the STM32H563 microcontroller as an example.  This guide is divided into two parts: Prerequisites This project utilizes the following so...

STea_6-1720537723656.png STea_0-1720535182402.png STea_5-1720537622676.png STea_4-1720537595677.png
STea by ST Employee
  • 6043 Views
  • 0 comments
  • 5 kudos

Tips for using STM32 low-power modes

Introduction For those developing applications that use low-power modes, trying to achieve the current consumption numbers listed in the datasheet and performing general debugging can be troublesome. The purpose of this article is to give an overall...

MCUSupportTD_0-1702918556927.png MCUSupportTD_1-1702918713976.png MCUSupportTD_0-1702918956534.png MCUSupportTD_1-1702919543374.png

FAQ: How to configure FIFO with the OCTOSPI interface

Maximum FIFO size with the OCTOSPI interface The FIFO is sized into the targeted product, typically either 32 or 64 bytes depending on the product. Refer to the reference manual to check the maximum size in the "FIFO and data management" section. Co...

KDJEM.1 by ST Employee
  • 1814 Views
  • 0 comments
  • 2 kudos

How to measure the junction temperature of an STM32H7

The STM32H7 MCU family clock reaches up to 600MHz and thermal management matters due to power dissipation, see details in the AN5036 Guidelines for thermal management on STM32 applications. https://www.st.com/resource/en/application_note/an5036-guid...

BartoszBORYNA_1-1720168897764.png BartoszBORYNA_2-1720169006997.png BartoszBORYNA_0-1720169116141.png BartoszBORYNA_1-1720169175103.png

Debugging tips when working with an Ethernet peripheral

Introduction In this article, we discuss some debugging tips when the Ethernet is not working as expected. When working with the Ethernet peripheral on an STM32 either through a custom board and firmware or with one of ST provided boards and middlew...

ST800_18-1719223045960.png ST800_19-1719223045962.png ST800_20-1719223045965.png ST800_21-1719223045967.png
STea by ST Employee
  • 4608 Views
  • 0 comments
  • 2 kudos

How to use NanoEdge AI Studio for anomaly detection

Summary This article offers a quick guide on how to implement anomaly detection using NanoEdge. It provides a step-by-step tutorial accessible to AI novices on how to use the tool. The demo implemented is based on a simple orientation detection appl...

BMontanari_0-1721075516572.png BMontanari_1-1721075827123.png BMontanari_2-1721076253575.png BMontanari_3-1721076336649.png

How to use NanoEdge AI Studio to create a data logger

Summary This article presents a comprehensive guide on utilizing NanoEdge AI Studio to develop a data logger for embedded projects on Arm® Cortex® -M MCUs. It addresses the essential prerequisites, initiates a project with data logger generation, an...

BMontanari_2-1721074696402.png BMontanari_3-1721074807659.png BMontanari_4-1721074911136.png BMontanari_5-1721074971252.png

How to solve debugger connection issues

Introduction The debugger is a tool that permit the programmer to monitor and track its code. It is very useful to execute the code step by step and see how it responds, it also helps to indicate the source of an error in case of malfunction.The debu...

1481.png 1482.png 1483.png 1484.png

CAN reception issues: Reasons and general troubleshooting

Introduction CAN bus is a robust protocol to transmit/receive data. It can be very sensitive to any issue that could lead to communication errors or even halt communication. STM32 users need to have a basic knowledge of the CAN bus (protocol + hardwa...

can-bus-bit-rate-vs-bus-length.png
mƎALLEm by ST Employee
  • 8535 Views
  • 0 comments
  • 4 kudos