NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Dear Community,after the most recent Webinar regarding LoRaWAN Relays I downloaded the newest CubeWL, which was version 1.5.0 and now I'm trying to migrate my code from CubeWL 1.3.1 to 1.5.0.My project is the Firmware for LoRaWAN Class C end nodes - ...
The WL series is great, but unfortunately there aren't any chips with more than 256KiB flash and 64KiB RAM. This appears to be a serious limitation for a SoC with LoRa connectivity.The value proposition of this series is that you pay for one package ...
Hi I have an app working perfectly on a Nucleo board and the MB2032 for the STM32WB05. Just the standrd default setup there.I have built my own board now following the application notes and the guides. It all starts ok but as soon as it gets to the a...
Hi,I developed PCB with STM32WB5MMGH6TR. I have code which I used previously with STM32WB55RG (on Nucleo board). I adapted it for STM32WB5MMGH6TR and it works (GPIO, SPI, I2C) except the BLE part. So I took STM's BLE_HearRate example for STM32WB5MM-D...
Dear STMicroelectronics Team,We would like to request clarification regarding the delivery schedule of our STM32WL5MOCH6TR orders.As indicated in the attached correspondence and supply reports, we were initially informed that our order would be deliv...
Hello,On the STM32WL3R microcontroller, when deep stop mode is activated, the current consumption is about 1.3 mA, which is a very high value compared to the 0.8 µA specified in the datasheet. In contrast, when I activate shutdown mode in the same fi...
Hi everybody, I have an application, where my device should go every record_interval into the stop2 mode. Then Wakes up then measure some sensor values, then goes into the sleep. Same goes over and over. The issue is, I am using the LSI2 as a clock s...
Hello everyone, I have my own custom board based on the STM32WLE5CC , and I want to build a LoRaWAN project on it. For the RF design, I used the MB1874-LP reference schematic as a base, together with the BALFHB-WL-06D3 balun/filter for a 2-layer PCB,...
The problem I am facing is that I can't seem to get passed the SystemClock_Config() function call, more specifically, the HAL_RCC_OscConfig() function returns HAL_TIMEOUT in this part indicating that the HSE is not getting ready. /* Wait till...
Dear Experts, I have an E04-400 module which contains a 48 MHz tcxo controlled through PB1 pin.If i set the module to use HSI it can work (blinks an LED, radio is off)If i set the module to use HSE (and set PB1 to 1 directly when main.c starts) the m...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.