STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575 Boot up power consumption

Hi All, I am trying to reduce the boot up power consumption using STM32U575RIT6xQ . I using a 4-20mA power source and the boot up power is 7.6mA. After it boots up the power consumption is 3.4mA. We are using Free RTOS. Below is the pins that are act...

Jet1 by Associate II
  • 1046 Views
  • 1 replies
  • 0 kudos

Resolved! Typo in STM32C0 reference manual?

On page 1017, Section 31.3 in Package data register of the STM32C0 reference manual (Revision 5), looking at the PKG[3:0] bitfield, when the condition is STM32C071xx, there seems to be two parameters with the same value? Was the value 0b1100 intended...

ivanmak_0-1744226648454.png
ivanmak by Associate
  • 1163 Views
  • 2 replies
  • 1 kudos

STM32U585 BACKU RAM VBAT RETENTION ISSUE

We are using the part STM32U585 controller in our board and we have designed it with battery backup support of 3.0v We are evaluating the backup ram (address 0x50036400)performance and found that it is not able to retain the information on power down...

SAI Configuration on STM32H5

I am trying to use the Nucleo H563ZI to read a 24 bit data via the SAI with the TDM protocol. SAI has been configured in asynchronous slave mode. Valid data from the master is available after the falling edge of the FS signal. However, while calling ...

stmexplorer_1-1744206053842.png stmexplorer_0-1744205911107.png

Resolved! Two VREF+ pins on STM32G474Q?

When I first glanced through the STM32G474 datasheet, I saw VREF+ and VREF- on pins 43 and 44 on the LQFP128 package. "Cool", I thought, although I had no significant need for an actual VREF- pin.However, when I was making a schematics symbol, I noti...

EThom3_0-1743606269300.png
EThom.3 by Senior III
  • 4666 Views
  • 13 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.