2025-04-09 12:35 PM
Hi All,
I am trying to reduce the boot up power consumption using STM32U575RIT6xQ . I using a 4-20mA power source and the boot up power is 7.6mA. After it boots up the power consumption is 3.4mA.
We are using Free RTOS. Below is the pins that are activated :
1. ADC1 3 Channels
2. GPIO 26 Pins
3. I2C2 2 pins
4. TIM 2 timers
5. UART4
6. USART3 Asynchronous
My requirement is the device should boot up and run below 3.5mA. Is there a way to reduce it in the firmware at the boot up.
I am aware that power saving mode can be implemented in the code but not sure how to reduce power at boot up. If anyone could provide any assistance it would be very helpful
Thank You in advance
2025-04-10 7:27 AM
Hello @Jet1,
Referring to the dedicated reference manual, the power consumption in Run mode can be reduced by one of the following means:
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.