| Subject | Author | Posted | |
|---|---|---|---|
|
Hello, I'm having trouble getting a lock with the DCMI. Lots of information below as required. Ha...
| 2026-06-07 11:21 AM | ||
|
Hi ST Community, I'm working on a custom board with STM32N6, and I plan to connect 4 MEMs micropho...
| 2026-06-05 8:58 PM | ||
|
Hi All, I'm working on an STM32N6-based board for speech recognition with Direction of Arrival (Do...
| 2026-05-31 2:58 AM | ||
|
I am writing code for a system where a STM32F1 communicates with the 8-bit data bus of another CPU ...
| 2026-05-24 4:23 AM | ||
|
Building a very interesting platform on U545. It requires Trustzone, will provide PKI stuff, lets s...
| 2026-05-23 7:05 PM | ||
|
Hello everyone, I have an NUCLEO-H755I-Q with the following setup; i) A 50Hz PWM input pulse goes...
| 2026-05-06 7:24 AM | ||
|
When TxRSTU and RETRIG are enabled with CONT disabled, will the timer still trigger a register ...
| 2026-05-03 10:27 AM | ||
|
Hi, Any reason why the GBW of the OPAMP is having such a wide tolerance? Is it purely because the ...
| 2026-04-08 4:19 AM | ||
|
We had: An STM32H7Sx with an external flash on one XSPI port, and an external RAM on the other; ...
| 2026-03-13 8:54 AM | ||
|
Greetings,
I am working with the STM32U585RI and a sensor that asserts an interrupt on the MISO l...
| 2026-03-03 12:12 PM | ||
|
Hello everyone!
I got the following problem; I need to read from two 32bit addresses and writ...
| 2026-02-16 7:09 AM | ||
|
Hello STM32N6 Tech support
I am writing with reference to power on sequence. My power sequence is...
| 2026-01-20 4:39 AM | ||
|
Hello
I would like to build a full bridge converter according to attached topology picture. The s...
| 2026-01-06 2:32 AM | ||
|
I am using I2S (SAI) on the STM32L433 nucleo board and using the internal MSI RC as the clock sourc...
| 2025-12-17 12:41 PM | ||
|
Hello, I have application which go to STOP2 mode once no LPUART/Modbus communication (Running at 3...
| 2025-12-16 10:20 PM | ||
|
Hello, I'm working on finding the smallest possible power solution for the STM32N6. The refer...
| 2025-10-14 5:44 AM | ||
|
Post edited by ST moderator to be inline with the community rules especially with the code sharing....
| 2025-09-17 10:02 AM | ||
|
I connected the nucleo board with the cpu using port CN6 using USB-C cable with BOOT0 and BOOT1 set...
| 2025-09-08 12:28 AM | ||
|
Hello, When using stop mode 3 with the stm32u5a9j chip, I noticed a unexpected behaviour when exit...
| 2025-08-26 2:40 AM | ||
|
Dear ST Community, I am using the STM32H573's SDMMC interface to communicate with a soft eMMC devi...
| 2025-08-07 7:47 AM |