2025-03-10 10:45 PM - last edited on 2025-03-11 9:55 AM by Peter BENSCH
We are using the part STM32U585 controller in our board and we have designed it with battery backup support of 3.0v
We are evaluating the backup ram (address 0x50036400)performance and found that it is not able to retain the information on power down
Initialization routine
1)MX_RAMCFG_Init();
2)__HAL_RCC_PWR_CLK_ENABLE();
3)HAL_PWR_EnableBkUpAccess();
4)RCC->AHB1ENR |= RCC_AHB1ENR_BKPSRAMEN; // Enable backup RAM retention
5)PWR->BDCR1 |= PWR_BDCR1_BREN; // Enable backup RAM retention
6) PWR->BDCR1 |= 1; // Enable backup RAM retention
test procedure
1) write the test value at address 0x50036400
2)power down the board
3)power up the board
4)read the content at address 0x50036400
5)check for the test value
but, it returns garbage value though we attempted this trials few times
Kindly support us in solving this issue
2025-03-12 3:45 AM
What is the VBAT voltage while your board is in power down mode? You need to maintain a voltage on VBAT higher than 1.65V when it no longer supplies VDD.
You can also refer to the Application Note AN5373, specifically the section "2 Power Supply Management" which can help you.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-10 5:33 AM
Hi ELAB1
Thanks for your reply
It is 3.2V battery
Thanks
G.Vaikundam
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.