STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743 problem with sdcard clock

Hey,I have a chinese STM32H743 Board, with a 25Mhz Clock Source and sdcard 3.3V VDD.my clock settings:my SDMMC1 config:static void MX_SDMMC1_SD_Init(void) { /* USER CODE BEGIN SDMMC1_Init 0 */ /* USER CODE END SDMMC1_Init 0 */ /* USER CODE B...

clock1.png clock2.png
Sany by Associate III
  • 1679 Views
  • 3 replies
  • 0 kudos

Boot from the bootloader with nucleo h7s3l8

Hi all, I am using the NUCLEO-H7S3L8 board, and trying to boot MCU from the bootloader.Based on the reference manual, the conditions for that at the MCU reset :PRODUCT_STATE = OpenNVSTATE = OPENBOOT0 = HighI checked PRODUCT_STATE = Open at the option...

Daewoong by Associate II
  • 2160 Views
  • 4 replies
  • 0 kudos

What is the VBAT function?

If the PDR_ON connector is connected to the GND, the VBAT function may not be available.What is the VBAT function?To use RTC, a coin cell is connected to the VBAT connector. Is there a problem if the PDR_ON connector is connected to the GND?I am usin...

Kazuhiro by Associate II
  • 2210 Views
  • 4 replies
  • 3 kudos

STM32H753 - LSE Drive Strength and GPIO Speed

Hi Team, We are using the STM32H753 in our design.For the signal quality, we are adjusting the LSE drive strength.Below are the four options available in drive strength,low drivemedium low drivemedium high drivehigh driveKindly let us know drive curr...

SAI Problems in slave receiver mode

Hello,I am trying to read sample from a AD7768 using a STM32F767. The data is feed to the SAI peripheral at 8Mhz. I used this code https://github.com/pavel-demin/stm32f7-discovery-usb-headset/blob/master/Drivers/BSP/STM32746G-Discovery/stm32746g_disc...

mickael2 by Associate II
  • 4458 Views
  • 3 replies
  • 1 kudos

Using SAI on the STM32H5

Hello Team , I am trying to use the SAI1_A on the STM32H563ZI and I am not able to read any data using the asynchronous RX Mode. The control keeps checking for status != SAI_FIFOSTATUS_EMPTY and there are no updates post that.(Although, I am using th...

Jansunil_0-1701939515169.png
Jansunil by Associate II
  • 1556 Views
  • 1 replies
  • 0 kudos

STM32F401 Stop Mode entry

Posted on April 11, 2016 at 13:32Hello,I'm currently working on an application in which I need to put the MCU into the STOP mode, being able to wake it up by means of an EXTI. However, I'm having difficulties putting the MCU to STOP using __WFI(). I...

jesper2 by Associate II
  • 4229 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.