2025-04-07 2:35 PM
Hi,
I try the whole day with an F103C8 to have the Alarm Pulse on Tamper Pin C13 but it is not possible, I tried with PullUp resistor and also I tried to configure manually the GPIO Pin to AF OD config. But with my Osciloscope I cannot see anything. Only works the Clock divided with 64 output, with this configuration I can see the clock with a 511Hz signal. I tried CubeIDE 1.15 and 1.18 with tha same results.
Any Ideas?
Kind regards,
Niko
2025-04-08 2:45 AM
Hello @NTosi,
Could you share the RTC configuration that's not working?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-08 4:04 AM
2025-04-10 6:05 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.