STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Function HAL_PWREx_EnableVddUSB() for STM32C0 series MCU

Hi,I am implementing USB CDC ACM on my custom board using STM32C071x series of microcontroller. It is currently not working and looking at other post on community I observed that one of the problem is of missing call to function - HAL_PWREx_EnableVdd...

PPate.1 by Associate III
  • 1287 Views
  • 1 replies
  • 0 kudos

Custom STM32H755ZI board not working

Hello everyone, I'm facing an issue with a custom PCB I made using the STM32H755ZI.I also own the nucleo board for the MCU, so I'm sure the program works well; it's just a blink program.The power schematics are inspired by the nucleo board schematics...

STM32H563 RADC value

Please let me know STM32H563's RADC value.There wasn't RADC value on datasheet of STM32H563. STM32F427's datasheet have RADC value.Best regards,

tomy_0-1743498039679.png tomy_1-1743498103704.png
tomy by Associate II
  • 1251 Views
  • 2 replies
  • 0 kudos

物料型号:STM32C071GBU6N,品牌:ST

您好! 物料型号:STM32C071GBU6N,品牌:ST,因数据手册未写明对应主丝印,烦请帮忙确认主丝印是否为“C071B6N”,谢谢! Translation: Hello! Material model: STM32C071GBU6N, brand: ST. Since the data sheet does not specify the marking, please help confirm whether the marking is "C071B6N". Thank you!...

WuZunMing_0-1743056910151.png

STM32H7 timer is too slow

Hi,I'm using STM32H755 Nucleo board and I'm trying to use TIM2 to trigger Dual ADC conversion. M7 core is running FREERTOS and M4 is bare metal. ADC is controlled by M4 core. DMA is used to transfer data to M7 and then M7 is using ethernet to transfe...

clock.PNG TIM2.PNG
mosamasa by Associate II
  • 2233 Views
  • 6 replies
  • 0 kudos

Resolved! STM32G0B1CCT6 FDCAN Bootloader

Hello, According to reference manual/datasheet/ANs, it exists some documents that are pointing out that FDCAN2 is the capable bootloader port for upgrade.In ANs and reference manual, it is specified that FDCAN bootloader mode is available on PD0 & PD...

RomainP by Associate
  • 1472 Views
  • 3 replies
  • 3 kudos

Bootloader on STM32H730 with FreeRTOS

Hi everyone,I’m currently facing an issue related to bootloaders and FreeRTOS on STM32 microcontrollers, specifically the STM32H735 and STM32H730.Here’s the background:STM32H735 Development Board: I have successfully implemented a bootloader that jum...

HispaEmo by Associate III
  • 1543 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.