2025-04-01 6:20 AM
Hello,
According to reference manual/datasheet/ANs, it exists some documents that are pointing out that FDCAN2 is the capable bootloader port for upgrade.
In ANs and reference manual, it is specified that FDCAN bootloader mode is available on PD0 & PD1 related to FDCAN1 instance.
Can you confirm please?
Thank you
Solved! Go to Solution.
2025-04-01 6:49 AM
AN2606 only lists FDCAN1 and PD0/1.
2025-04-01 6:49 AM
AN2606 only lists FDCAN1 and PD0/1.
2025-04-01 7:48 AM
The RM0444 rev5 Section 3.3 was mentioning FDCAN2. But the updated version rev6, is now forwarding to AN2606
2025-04-01 9:08 AM
If RM0444 silently drop the not without a note in the revision history, that is ugly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.