STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DBANK Option Byte default STM32G4

What is the default value of the DBANK bit in STM32G4 MCUs. According to the reference manual, flash memory address 0x1FFF 7800 has that option bit, and the ST production value is 0xFFEF F8AA, which would make DBANK default to 1. Does this mean STM32...

tomm5771 by Associate III
  • 1360 Views
  • 2 replies
  • 1 kudos

Resolved! GP and N version ICs

Hi,I am using STM32C071CBT6 chip on my custom board. From datasheet, i could see that there are two versions available - GP and N version. Part number section of datasheet mention about 3 more characters after this part no. to identify if it is N ver...

PPate1_0-1743594616574.png PPate1_1-1743594767820.jpeg
PPate.1 by Associate III
  • 1318 Views
  • 1 replies
  • 0 kudos

Resolved! Implementing STM32L4S5ZIT6 Bootloader with a Memory Marker

Hello, I am working on the development of a bootloader for the STM32L4S5ZIT6, and I need help to implement a feature where the bootloader is triggered after receiving a user request in the main application (the main app saves a marker in memory). Her...

ZAYN by Associate II
  • 1389 Views
  • 2 replies
  • 2 kudos

Help with Ethernet on STM32 H723ZG

Hi all! I have been using a F446RE board to communicate with an encoder using SPI. I get back a 16-bit value every ms (the process runs at 1kHz). However, I now need to transfer the acquired data over ethernet (it has to be ethernet, not UART or anot...

Screen Shot 2024-06-21 at 2.07.16 PM.png Screen Shot 2024-06-21 at 2.07.44 PM.png Screen Shot 2024-06-21 at 2.08.06 PM.png Screen Shot 2024-06-21 at 2.08.19 PM.png
shuyu_vk by Associate
  • 4603 Views
  • 5 replies
  • 2 kudos

Resolved! AN5306,STM32G431: OPAMP output connected to both ADC's internal channels and external pins

在本文的第 32 页,图 38 显示了双电机控制应用的概述。 其中 OPAMP2 通过内部多路复用器连接到 ADC2IN16, 它还输出到外部引脚 PA6,该引脚通过附加线路连接到 ADC1IN1/PA0。 Translation: "On page 32 of this article, Figure 38 shows an overview of a dual motor control application. Where OPAMP2 is connected to ADC2IN16 ...

屏幕截图 2025-04-02 090425.png 屏幕截图 2025-04-02 090412.png

FMC initialising and RTC desactivation

 Dear All, I designed a HMI board with STM32F767 and QSPI NOR flash and MT48LC16M SDRAM with external OSC 8MHz and MC-306 32.768 KHz.Approximately I tested more than 100 PCs of this board and all work without any problem. but during this week in some...

HamedAth by Associate
  • 1046 Views
  • 1 replies
  • 0 kudos

Resolved! LPTIM2 not counting when clocked from PLL2P on STM32H563

Hi I'm doing a new design using an STM32H563 and would like to use LPTIM2 to measure elapsed time. Ideally I'd like its clock source to be PLL2P, which means RCC->CCIPR2.LPTIM2SEL = 0b001 according to RM0481 page 545. However, if I select this clock ...

andy by Associate III
  • 1129 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.