STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SAI: SPDIF output in all MCUs ?

Heyho,do all SAIs in all MCUs offer the SPDIF output feature?CubeMx and online MCU selectors do not show this info, no time to check 20 more datasheets.For the few STM32 I know and worked or played with (G4, F7, H7) the answer is yes.Merci!

LCE by Principal II
  • 1262 Views
  • 8 replies
  • 2 kudos

STM32N6: External Loader Manager, ISSI Flash

Hello,Hello, in our project we are using an STM32N6 MCU and an external flash from ISSI with this MCU. Datasheet of the flash's link in the below.https://www.issi.com/WW/pdf/25LX-WX032-064.pdfDuring debugging, we read the flash using standard command...

Clyasenth_0-1748356963697.png Clyasenth_1-1748356982432.png
Clyasenth by Associate II
  • 1350 Views
  • 2 replies
  • 0 kudos

STM32F407 RAM Interface impedance matching

Hi Team,As we are going to use RAM – IC CY62136EV30 (TSOP-44) in our new project with ST micro STM32F407ZG (LQFP-144).Do we need any impedance matching for 6-layer board?Can you please suggest the same. Crystal frequency we taken 16MHz for the MCU.Th...

Resolved! STM32N6: Expected DMA/SPI Performance

Hi,I am working on an application for the STM32N6 (using zephyr) that streams data from four SPI interfaces (SPI1, SPI2, SPI3 and SPI6) via Ethernet (UDP). I am using full-duplex SPI transfers and GPDMA1.Everything works fine up to SPI clock frequenc...

Jeija by Associate
  • 773 Views
  • 1 replies
  • 0 kudos

Resolved! DCMIPP Capture Buffer Not Receiving

Hello,I’m currently testing the CSI–DCMIPP interface on the Nucleo-N6 board. I’m following various examples, but the variable used in DCMIPP_Start (lcd_bg_buffer) is not receiving any data. Is there something I might have configured incorrectly?At th...

silpiode by Associate II
  • 693 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G051c8t6 PA5 Not working as GPO

I turned off all the other configuration aka Alternate Functions..only enabled GPIO PA5 as output Pushpull mode, low freq.its doesnt turn on or off individually..tried to turn on and off using HAL as well as direct registers..both work only when PA4 ...

Screenshot 2025-11-21 103226.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.