2025-11-14 3:42 AM
Hi Team,
As we are going to use RAM – IC CY62136EV30 (TSOP-44) in our new project with ST micro STM32F407ZG (LQFP-144).
Do we need any impedance matching for 6-layer board?
Can you please suggest the same. Crystal frequency we taken 16MHz for the MCU.
Thanks.
Regards,
Ashutosh
2025-11-14 8:32 AM
Having short traces is most important.
Then length matching. Differences up to a couple cm are generally fine.
Then impedance matching. If traces are short, this matters very little.
2025-11-15 5:11 AM
Thanks for the feedback!
I mean do we need any series resistance (22E or 33E) to be added in data & address line or only shorter distance is enough with length matching on PCB routing? Kindly suggest the same.
2025-11-19 7:53 PM
Hi Team,
Can you please confirm on above mentioned?
Thanks.
Regards,
Ashutosh
2025-11-22 6:50 AM
Dear @ashutosh211 ,
You can check our Application Note AN4803
”High-speed SI simulations using IBIS and board-level simulations using HyperLynx® SI on STM32 MCUs and MPUs”
all depends on your Frequency speed of clock and data of the RAM I/F.
Hope it helps you ,
STOne-32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.