STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32N6 Core is locked

So i'm following along with this video* https://www.youtube.com/watch?v=usQ_f6Swpok&list=PLTJzs51NlEICI7ARAHOyUqMhTgJE0UFv0&index=5 I have the same* STM32N6-DK board This is my build command for the GPIO_IO_Toggle application.* /opt/st/stm32cubeide_1...

TheCoreIsLocked.png ProgrammingOutput.png

TIM 1 Advanved timer sometimes goes high

Hey!I will explain my setup and then paste the code. I have three different timers (TIM1, TIM2, TIM3) sending out PWMs to different parts of my board. All timers are set up the same way; the only difference is that TIM1 is an advanced timer.What I do...

morris by Associate III
  • 956 Views
  • 6 replies
  • 1 kudos

Resolved! STM32U5 SPI3 (SmartRUN domain) + GPDMA

On a stm32u5, the SPI3 is in the SmartRun domain, which is designed to work down to STOP2 in autonomous peripheral mode with LPDMA. I'm now wondering if it is also possible to use SPI3 in autonomous mode with GPDMA but only to STOP1? Or do I need to ...

bearsh by Associate II
  • 461 Views
  • 2 replies
  • 0 kudos

Resolved! Enumeration_USB_VBUS

Hello,let say that STM32H753 mCU has connected VBUS (via resistor divider to be sure that voltage on VBUS detection pin (PA9) would never exceed AMR), D-, D+ and GND lines with PC, before mCU core is supplied. At the moment when mCU core is then conn...

D3jan by Associate II
  • 766 Views
  • 4 replies
  • 0 kudos

Resolved! MIPI-DSI: Low Power Command Transmission

Hello! I'm now using a STM32F469 to drive a screen with MIPI-DSI Interface. I need to send the initial codes with low power command transmission, and then drive the screen in video mode. I think LPDT it is supported by this MCU, but I'm not sure how ...

123scy321 by Associate II
  • 1006 Views
  • 3 replies
  • 0 kudos

STM32F427ZGT6 inaccurate delay

Hello, when I was using this chip, STM32F427ZGT6, it could print data, but the delay was incorrect. After 5 seconds, it was only a few milliseconds. Due to the inaccurate delay, the timing sequence became disordered

liwei11 by Associate
  • 566 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.