STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32l151c8t6a device marking with QR code

Hi, I bought 50pcs STM32L151C8T6A from one Chinese online vendor, which has device marking with QR code.I encountered an issue while using the new version chip, after initial power-on, the overall sleep current of the product is approximately 5uA(STM...

owen_chen_0-1763653398218.png owen_chen_1-1763653463367.png

Resolved! STM32H747 Memory Mapped NOR-Flash AT25SF128A

Hi,I'm trying to implement an external loader for the Arduino Giga R1 board with AT25S128A 128Mbit of external flash. After following the guide given in the external loader repo, I'm running into the problem, that I can erase, write & read from the m...

Resolved! SIGTRAP when reducing HCLK

I'm in the middle of attempting to reconfigure the clock tree on my STM32F303K8. The old clock tree looks likeThe new clock tree looks like The old clock tree works fine. The new clock tree always fails on boot; not always in the same address but alw...

avidroneg_2-1763587965046.png avidroneg_1-1763587843385.png avidroneg_0-1763587716010.png avidroneg_3-1763588519230.png
avidroneg by Associate III
  • 1276 Views
  • 9 replies
  • 2 kudos

stm32h74 Errata: Max CPU frequency, and SPI

Hi Team,I have few questions regarding stm32h7 errata.Errata 2.2.21, Can silicon revision 'V' support a cpu frequency of 480 Mhz ? If yes, why is it showing 'P' for v revision.    2. Can I please ask if there is a fix in the HAL for the below given S...

Alex_001_0-1763659082288.png Alex_001_1-1763659307860.png
Alex_001 by Associate
  • 472 Views
  • 1 replies
  • 0 kudos

USB-C audio port and charging

HI USB-C Input (5–20 V PD) + USB-C Data (USB2.0 D+/D– to STM32H745) + charging phone at same time + Audio data transfer Problem: When I connect the USB-C input supply (PD 5–20 V), the phone only charges and the audio USB port does NOT appear.But when...

VIJAY212_1-1763640168685.png VIJAY212_0-1763640112560.png
VIJAY212 by Associate
  • 523 Views
  • 1 replies
  • 0 kudos

Resolved! SDMMC+MDMA withou FATFS on STM32H723ZG

Hello everyone,This is my first post on the platform, so please bear with me.I would like to write raw data to an SD card very quickly.After quite a bit of research, I decided to use SDMMC with MDMA, and I want to write directly to the SD card blocks...

davinci by Associate
  • 676 Views
  • 1 replies
  • 0 kudos

HSE clock setup issue on STM32H753-EVAL board

I'm trying to port a proprietary code that is designed for another STM32H753 plateform, to a STM32H753-EVAL board.My code remains stuck waiting for HSERDY bit.The setup I am doing looks identical to STM32CubeHW example but I guess I forgot something:...

Gpeti by Senior II
  • 520 Views
  • 1 replies
  • 0 kudos

How to drive the VD55G0 in N657B0

I want to use N657B0 to drive VD55G0, and the camera side can already enter the Stream state. After I use the function HAL_DCMIPP_CSI_PIPE_Start, I track the variable csi_instance through single-step debugging and find that several bits in its SR1 re...

eureka by Associate II
  • 851 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.