STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Confusion about STM32H7S3I8T6 OTG_FS_VBUS, HSE, and VCAP

Hi! I'm confused about the wiring for some of the pins on the STM32H7S3I8T6:  Does the full-speed USB connection require an external high speed oscillator?There's a GPIO that senses VBUS from USB called "OTG_FS_VBUS." Currently, we have it pulled up ...

ZitongW1 by Associate
  • 626 Views
  • 2 replies
  • 2 kudos

Resolved! Unable to use SMPS on STM32U375CGUxQ

I'm currently trying to configure a project based on an STM32U375CGUxQ, but I can only "choose" the LDO, even though the package clearly shows the SMPS pins:I'm using the STM32U3 package version 1.2.0, STM32CubeIDE 1.19.0, build 25607_20250703_0907. ...

cjb89_0-1754564353482.png cjb89_0-1754564803763.png
cjb89 by Associate II
  • 735 Views
  • 5 replies
  • 1 kudos

STM32H563ZIT6 - External memory not working

Hello,I have custom PCB based on STM32H563ZIT6 with external memory MX25L51245G(W25N01xx in schem.) and Riverdi display. I use ExternalLoader from https://github.com/cturvey/stm32extldr/tree/4dcb141b9cf6da2ee3fddf154d073bb6218a52e5/h5_mx25l51245g. Pr...

x-nucleo-plc01a1

Posted on May 23, 2018 at 16:45Hello, I am trying x-nucleo-plc01a1. but there are two jumpers (J5 and J11) on the board. I can't find any document to describe how to use them. Anybody can help?thank you.

yang hong by Associate III
  • 2418 Views
  • 6 replies
  • 2 kudos

Resolved! STM32G474RET Linker Question

In the linker script provided by STM for STM32G474RETx, the memory section is:MEMORY { CCMSRAM (xrw) : ORIGIN = 0x10000000, LENGTH = 32K RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K FLASH (rx) : ORIGIN = 0x8000000, ...

Resolved! STM32L432KCU CAN-RX Interrupt not firing

Hello there I am struggling with receiving interrupts on my microcontroller project. I am currently developing a CAN bus logging device; the following code therefore sets up the CAN peripheral in silent mode. I test my device in a CAN network with tw...

Resolved! RTC; code code get stuck in systemclockconfig()

we are observing with the RTC (Real Time Clock) on the STM32L496ZG in our project. kindly help us to resolve this . The code gets stuck on power-on . Below are the details and what we have tried so far:1. Summary of the IssueAfter a full  powering on...

Resolved! stm32g030 External crystal pin map

Hi everyoneI use STM32G030. I'm gonna set the clock system to HSE on the External crystal, but I couldn't find the proper RCC_OCS_OUT.What are the MCU's crystal correct pins?Please help me set the correct pinout.Thank you  

MTora1_0-1764336950376.png
MTora.1 by Associate III
  • 720 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.