2025-08-07 4:04 AM - edited 2025-08-07 4:06 AM
I'm currently trying to configure a project based on an STM32U375CGUxQ, but I can only "choose" the LDO, even though the package clearly shows the SMPS pins:
I'm using the STM32U3 package version 1.2.0, STM32CubeIDE 1.19.0, build 25607_20250703_0907.
Are there any prerequisites to being able to use the SMPS, and if so, what are they?
NB: There doesn't seem to be a "Power saving mode" under the PWR category:
Solved! Go to Solution.
2025-08-07 4:08 AM
Hello @cjb89 ,
Similar issue is reported here.
I confirm the issue. It is a STM32CubeMX issue.
I reported internally for correction.
Internal ticket number: 214214 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-07 4:08 AM
Hello @cjb89 ,
Similar issue is reported here.
I confirm the issue. It is a STM32CubeMX issue.
I reported internally for correction.
Internal ticket number: 214214 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-07 4:12 AM
Thank you. Is there a foreseeable time until the fix is deployed or some workaround?
2025-08-07 5:06 AM
Hello @cjb89 ;
I will keep you up to date until the issue is solved.
Thanks
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-01 12:25 AM
Hello @cjb89 ;
The issue is fixed in STM32CubeMX 6.16.0 version.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-01 1:30 AM
Thank you for the information; project is updated ;)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.