2025-12-01 3:59 AM - last edited on 2025-12-01 4:04 AM by Andrew Neil
2025-12-01 4:02 AM - edited 2025-12-01 4:08 AM
Hello @gaixin
You can use Both ST-Link V2 and V3. You just have to make sure that it is a genuine ST-LINK (specially for the ST-LINK V2).
Best Regards.
II
2025-12-01 4:03 AM - edited 2025-12-01 4:21 AM
@gaixin wrote:use stlink V2 or stlink V3?
Yes.
For a V2, just be sure to get a Genuine one.
You can see the full range of development tools on the 'Tools & Software' tab of the Product Page:
https://www.st.com/en/microcontrollers-microprocessors/stm32c091cc.html#tools-software
PS:
The full range of ST-Links is here:
See also: TN1235 - Overview of ST-LINK derivatives
Note that there are several variants of ST-Link V3 - from low-cost to fully-featured.
Even the cheapest V3 (STLINK-V3MINIE) is more versatile than a V2 - wider operating voltage range, and has a VCP (Virtual COM Port).
Note that the NUCLEO-C092RC comes with a built-in ST-Link.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.