STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Core supply for STM32H573MIY3Q

Hello,we have to use the STM32H573 in the 80 Pin WLCSP with temperature Range 3 (to 125°C). So STM32H573MIY3Q was chosen. Due to a mistake we didn't recognized that the internal LDO can't be used. Now we have no space for placing additional component...

MarwinS by Associate
  • 465 Views
  • 1 replies
  • 0 kudos

STM32L432 nucleo I2C bootloader communication issues

Hello,I'm trying to test FW update over I2C using RPI as host and STM32L432 nucleo board as slave on port I2C1 which according AN2606 (table 152) should be available. I've connected 4.7k pullups on PA6 + PA7 pins and perform NRST to 0 and BOOT0 to 1 ...

MBeli.1 by Associate III
  • 741 Views
  • 4 replies
  • 0 kudos

Resolved! What is the best PLL configuration for H533 ?

Hi there,I'm starting to use the NUCLEO-H533RE board to evaluate the H5 device family.RM0481 has some errors on the PLL configuration:Fig.55 on page 461 shows a VCO range 0 between 128 and 560 MHz, but the description of bit 5 of register PLL1CFGR (p...

Kraal by Lead
  • 873 Views
  • 5 replies
  • 3 kudos

Resolved! STM32N6 H264 Video Encoder ASIC datasheet / manual

Hello folks,I am investigating the Video Encoder on the STM32N6 and have been working through the reference project (VENC_SDCard_ThreadX).The user manual (RM0486) is very vague on detailing the Video Encoder, and lists over 100 pages of registers whi...

exarian_0-1745948663250.png
exarian by Associate III
  • 3977 Views
  • 9 replies
  • 6 kudos

NUCLEO-F103RB: Bare-metal USART driver

I'm writing a UART driver for NUCLEO-F103RB and I followed all steps in the book "Bare-metal embedded C programming" and advices from Gemini but still can't see the receiving output from my PC.How can I fix this?Other parts than UART work without pro...

1.png
Jajang01 by Associate II
  • 2037 Views
  • 10 replies
  • 8 kudos

Type III Format Interface Descriptor

Hi everyone!I figure out that Type III Format Interface Descriptor is generated automatically on STM32L476RG, and this use encoder format to transmit audio (Not PCM). Frame size vary an do mot match PCM packet sizes, meaning that transmitting  raw PC...

Resolved! STM32L0 inconsistency between RM0451 and CMSIS

Hi,I noticed that for the FLASH PECR register there is a discrepancy between the RM and the CMSIS files provided by ST.The RM includes information about the `NZDISABLE` bit (which is not present in the CMSIS file `stm32l010x6.h`). On the other hand, ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.