STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB PD Part selection

Hello, I'm working with the STM32U575VGT6 as my primary MCU and need a USB-C DRP PD IC. I'm considering the TCPP03-M20 or STUSB1600AQTR. My question is, when the PD operates in sink mode (during charging), we intend to turn off all power supplies, in...

Trigger SPI using Timer

I'm using STM32H723ZG I want to know if a Timer's update event can trigger SPI transfer without any software interrupts.This is the problem

STM32N6 External Loader

I'm currently developing an application with custom hardware using the STM32N657I0H3Q and MX25UM256, I can't seem to find the source files for the existing STM32N6 external loaders which use the MX25UM512. Any links to this or resources to point me i...

Resolved! STM32H742AG Flash Erase Bank 2 issues

Hello,I am trying to erase flash bank 2 and then re-write with an incoming application. This appears to work that when I read back some of this sector it's changed to 0xFFFFFFFF, however when I restart or connect with STLINK it reads out as 0x0000000...

kip18 by Associate III
  • 564 Views
  • 2 replies
  • 0 kudos

RTC Oscillator not stable

Hello,In one of our new PCBs we use a STM32L476VET6. For the RTC we use an external Oscillator (shown in the Picture)The drive power is set to the highest level.In our setup, the RTC only works at room temperature and with no probe connected. As soon...

FabianHladik_0-1731585469263.png FabianHladik_1-1731586045292.png

USB CDC device not recognized

Hello everyone. I am using an F411 and I cannot figure out how this is supposed to work. I enabled USB_Device in middleware, enabled USB_OTG_FS, and set up line encodings based on the default STM32 example, but when I flash STM (or step through with ...

Sandman2_0-1764225519675.png Sandman2_1-1764225567364.png
Sandman2 by Associate II
  • 1045 Views
  • 6 replies
  • 1 kudos

Resolved! Omit C29 and L1 in STM32WB55RGV6 SMPS design ?

Hello everyone,I’m working on an electronic design using the STM32WB55RGV6, and the final product cost is very constrained.I have a question regarding the SMPS components, specifically the capacitor C29 and the inductor L1 shown in the reference desi...

EndyQSM_0-1764264943373.png
EndyQSM by Associate
  • 563 Views
  • 1 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.