STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! Not able to use Port B alternate function (I2C)

Hi community,I am trying to use I2C on the STM32L010RBTX,during configuration in MX, i realized that when PB8 and PB9 is configured as I2C, the GPIO mode field shows n/a.And the I2C won't work as well.However, when i configure to PA9/PA10,GPIO mode s...

0693W00000LxM6wQAF.png 0693W00000LxM8xQAF.png
AWong.11 by Associate II
  • 4037 Views
  • 8 replies
  • 0 kudos

about stm32G070 TIM1

could a channel of TIM1 be configurated not only input mode but also output mode, so that it can capture a wave and generate PWM at the same time.

LOMO by Associate III
  • 1178 Views
  • 2 replies
  • 0 kudos

STM32F7 FMC SDRAM error after reinit

I have a custom board. There I have an issue with the FMC SDRAM after the HAL_SDRAM_Init call when calling it a subsequent(!!!) time. It works when doing the call the first time. I then deinit the SDRAM because of some current consumption tasks. When...

LFeld.1 by Associate
  • 2073 Views
  • 0 replies
  • 0 kudos

Resolved! HAL PWR Wakeup PINS do not match datasheet and cubemx.

Please tell me why the wakeup pin numbers are shifted up by one in the HAL PWR lib?See.. https://community.st.com/s/question/0D53W00001DKQdnSAH/wake-from-standby-not-working-stm32h753iit6?t=1637613024141If there is a legitimate reason for this mappin...

FColl.1 by Associate III
  • 4214 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.