STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CubeMX code generation: Keil project template

Posted on April 24, 2014 at 13:32Tired of changing project settings after each code generation from MX. Is there a chance of modifying Keil-project template? Thanks. #keil-cubemx-code-generation

jarno by Associate III
  • 1413 Views
  • 1 replies
  • 0 kudos

STM32CubeMX V1.1.0 + STM32F439 + FreeRTOS + LwIP bugs

Posted on April 24, 2014 at 04:50Greetings all,I have a couple of problems with STM32CubeMX-V1.1.0 with the following options: * STM32F439 * FreeRTOS * LwIP  The first problem is a bug in the sys_mutex_lock function which is generated as:    void sy...

malcolm23 by Associate III
  • 1266 Views
  • 1 replies
  • 0 kudos

Mixing Digital inputs and Outputs on the same port.

Posted on September 02, 2013 at 13:14Hi Folks I'm working with the 32F4 discovery board and I've been looking for some examples of mixed Input and output pins on the same port, however they seem a like hard to find!! I checked the Ref Manual and doe...

bl by Associate II
  • 8004 Views
  • 16 replies
  • 0 kudos

STMCube USB Host code not working

Posted on April 08, 2014 at 11:51 Hi, I can't get the USB Host code generated by STMCube to work. When I connect a device, none of the interrupts get triggered - the software doesn't seem to recognize it at all. The peripheral cl...

brett by Associate II
  • 3464 Views
  • 8 replies
  • 0 kudos

STM32CubeMx Bug - DMA interrupt

Posted on April 01, 2014 at 12:38 STM32CubeMx generate code for STM32F407VGTx I chek box '' DMA2 Stream0 global interrupt'' in '' NVIC Configuration'' STM32CubeMx not add in stm32f4xx_hal_msp.c - HAL_NVIC_EnableIRQ: ...

levak by Associate II
  • 3787 Views
  • 7 replies
  • 0 kudos

STM32Cube CDC - problems and a possible bug

Posted on March 22, 2014 at 01:39 Hello. I am currently trying to build a project using the STM32F429 iDisco. The toolchain I am using is the arm embedded gcc, under Eclipse IDE. I am trying to use STM32Cube to write the ini...

matteo by Associate II
  • 3649 Views
  • 9 replies
  • 0 kudos

ST32CubeMX project file for ST32F407 Discovery board

Posted on February 21, 2014 at 15:09Hi all,I have installed ST32CubeMX tool and I was wondering if there are any ''pre-built'' project files for STMicro evaluation boards such as ST32F407 Discovery board. I don't know the exact configuration of the ...

CubeMX Selecting timer Enocder Interface.

Posted on March 12, 2014 at 22:17I am trying to use the STM32CubeMX tool to select and generate initialization code for the encoder interface.  I am using the Discovery board (STM32F407VGT) and trying to configure timer 5, but not sure how to get it...

craig2 by Associate
  • 2038 Views
  • 2 replies
  • 0 kudos

Stm32F405 CubeMX code lead to Hardfault

Posted on March 04, 2014 at 19:42HiI'm exploring the STM32F405 and for this, i wanted to create the initial project with the Cube MX tool. I've settet all the things up to my configuration. In minimal i just set the hole clock thing up.I've burned t...

nico by Associate II
  • 2264 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.