STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 300 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4117 Views
  • 0 replies
  • 3 kudos

Resolved! Toggling LED on STM32WBA25CE1 in the task

I am using NUCLEO-STM32WBA25CE1. I created STM32CubeMX project for this board. I activated RF, WPAN, RTC. I configured a wakeup every 10 seconds and set up a task for the sequencer to toggle the LED. The LED pin is correctly configured. I can toggle ...

suiunbek by Associate II
  • 302 Views
  • 4 replies
  • 0 kudos

Resolved! PA0 WakeUp from Deep stop unreliable on STM32WL31

Good day. I am using STM32WL31 on a custom board.DeepStop mode entry works correctly, but wakeup from PA0 (WakeUp pin) is not reliable or does not work. I used the example code in project:STM32Cube_FW_WL3_V1.3.1\Projects\NUCLEO-WL33CC\Examples\PWR\PW...

Resolved! STM32WL31 fails to exit DEEPSTOP from RTC wakeup

Good day,I have a simple custom board with a STM32WL31 that needs to cyclically enter DEEPSTOP mode and then wake by means of RTC internal wakeup. It seems the device enters DEEPSTOP, but does not wake from it. Basic setup:Clocked from HSI, RTC clock...

marvdm by Associate II
  • 1756 Views
  • 14 replies
  • 3 kudos

NUCLEO-WB09KE board USUART -> LPUART change fail

Dear ST team.(related :Re: UART of NUCLEO-WB09KE UART signal no found - STMicroelectronics Community)I am testing with NUCLEO-WB09KE EVBStarted from the example code ; "BLE_Peripheral_Lite", which is using PB0/PA1 as usuart portI can see the Uart out...

JunkgyuHan_0-1778140574863.png 949988ff-e84c-4790-a866-6bd2194b8b12.jpg JunkgyuHan_1-1778140865069.png

Joining a LoRaWAN network only once

Can I join a LoRaWAN network only once?so that after a software or hardware reset, i would not need to join the same network once again I am working with LoRaWAN_End_Node_LBM example

onass by Associate III
  • 310 Views
  • 3 replies
  • 2 kudos

Resolved! Non standard preamble on STM32WL33

I need to implement a protocol using 11110000 as preamble. The protocol is 2-FSK 868.1 MHz, +/-35kHz, 25kbps. According to RM0511 STM32WL33 only supports 01010101 or 10101010 as preamble for 2-FSK. Is it feasible to use the STM32WL33? I am planning t...

DirkH by Associate II
  • 179 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.