NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Posted on November 07, 2015 at 16:48Hi, I ported an example from the stm32f4 cube lib for stm32f469I_eval board to a nucleo f411. I works quite well with a wired keyboard but does not work with a microsoft wireless keyboard. I thought that it may be...
Posted on November 24, 2014 at 20:10Hi, I'm using Dizic radio modules (STM32W108CB based ones) with SimpleMac v2.0.1 library. Overall, the example projects work with exception of packet transmission (802.15.4). Every time it accepts the packet trans...
Posted on July 11, 2014 at 19:01Hi, I would like to know if it would be better to send AT commands to the HC-06 Bluetooth module via an interrupt handler or a while(1) in the main as well as some pointers on the code I am trying to get correct and w...
Posted on June 23, 2014 at 12:01Dear all, Do you know whether ST provides network (RJ-45) and wireless shields (a/b/g communication) for the new Nucleo F401-RE / F411-RE platforms. I know these platforms are compatible with: Arduino Uno Revision 3...
Posted on September 24, 2011 at 01:45I read previous threads about source code. But how can i find source code related with UM0794: GSM interface?... Is there any link ? Should we contact local distributor for this? if it is so, why ? Thanks in adva...
Posted on March 18, 2013 at 05:29Hi All, Im after adding WiFi capabilities to my PCB (either onboard chip or shield) for the STM32F4. Basically the unit will need to connect to a network via DHCP and dump data from an SD card to the server. I'm usin...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.