2026-05-04 1:49 AM
I am using NUCLEO-STM32WBA25CE1. I created STM32CubeMX project for this board. I activated RF, WPAN, RTC. I configured a wakeup every 10 seconds and set up a task for the sequencer to toggle the LED. The LED pin is correctly configured. I can toggle the LED before the main loop starts. But in the task LED toggling is not working. How should i configure GPIO and anything else to get LED working?
I am using STM32CubeMX 6.17.0 and STM32CubeIDE 2.1.1 versions.
Moreover, I try to use USART1 or LPUART1 for debugging. Before the MCU goes into low power mode, i can output the message to the terminal. But after the low power mode it stops working.
Solved! Go to Solution.
2026-05-04 3:00 AM
Hi,
Which low power mode are you using?
Furthermore, I recommend that you take a look at basic projects such as the BLE_HeartRate, which uses low power and transmits data every second.
You can find the example here:
STM32CubeWBA/Projects/NUCLEO-WBA25CE/Applications/BLE/BLE_HeartRate at main · STMicroelectronics/STM32CubeWBA
BR, Joé
2026-05-04 2:14 AM - edited 2026-05-04 2:14 AM
Hello,
As admin, let me intervene here. You said in the title: "Toggling LED on STM32WBA25CE1 in the task".
What RTOS are you using? ThreadX, FreeRTOS? you didn't tell in your post.
Please review How to write your question to maximize your chances to find a solution
Also need to separate questions in the community. For the last question, please post a new thread for it.
Thank you.
2026-05-04 2:28 AM
Thank you for pointing me to the "How to". I will follow the recommendations next time.
I am using bare metal. STM provides the sequencer to manage various tasks. I created my own task to toggle the LED. I configured pins according to UM3610.
I think the second question is similar to this one. If i get this resolved i will check again if i need to post a separate post.
2026-05-04 3:00 AM
Hi,
Which low power mode are you using?
Furthermore, I recommend that you take a look at basic projects such as the BLE_HeartRate, which uses low power and transmits data every second.
You can find the example here:
STM32CubeWBA/Projects/NUCLEO-WBA25CE/Applications/BLE/BLE_HeartRate at main · STMicroelectronics/STM32CubeWBA
BR, Joé
2026-05-13 5:12 AM
Dear Joe,
thank you for the direction. I looked at HeartRate project. Although it does not use the wakeup timer (it uses an alarm), it is a viable solution for me. I think i can close this thread now.
Regards,
Suiunbek
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.