NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am currently working with the LoRa-E5 Mini module based on the STM32WLE5JC microcontroller, and I am using STM32CubeIDE version 2.1.0 for development. I have successfully tested basic GPIO functionality (LED blinking), and I am now trying to implem...
Board / SoCBoard: NUCLEO-WB09KESoC: STM32WB09SoftwareZephyr version: v4.4.0-rc2-41-g149c8b1758a8Toolchain / build system: West + Zephyr standard build flowIssue summaryWhen building a very small Zephyr application for NUCLEO-WB09KE, simply enabling:C...
Ok, a tricky one. So for services and attributes it's documented that there is 10752 bytes, each service takes up 48 bytes, each attribute 40 bytes, and if you got th number of services and attributes you can compute backwards BLE_ATT_VALUE_ARRAY_S...
Hi everyone,I am experiencing a very specific initialization issue with a custom board based on the STM32WB55RGV6.We recently manufactured a batch of 30 boards. 22 of them are working flawlessly, but 8 boards fail to start the BLE radio on a cold boo...
Hello,I have designed a custom board with stm32wb55. I used the reference schematic and checked everything but I cannot program the board from my cubeide. I have tried different configuration settings in Cube IDE but always got "No device on target" ...
Dear ST team. I am testing UART of NUCLEO-WB09KE with the board [STM32WB09 Nucleo-64 board (MB1801 and MB2032)] I Set UART1 PIN PB4, PB4 with the source attached[100ms period tx send ]. I am checking CN3(23), CN4(35) but no signal shown. Is there a...
Hello,I am currently working with the STM32WBA65RI for BLE Direction Finding using connectionless mode. I would like to know if it is possible to use a low-power mode such as Standby with RTC, allowing the board to consume only a few nanoamps, then w...
I am struggling with the keys in the new V1.5.0 LBM stack. Keys are read from NFC EEPROM and device is joining. After joining, I expect the stack to save the join and session keys in secure memory so the keys are deleted in EEPROM for security. After...
Hello. I'm working on a BLE application that uses an STM WBA55 board and ThreadX. It was based on the St Threadx p2pServer example, The Sequencer is disabled. I'm using stmCubeIDE 1.19 and st_fw1.7 and i cannot migrate to new versions due to compati...
Dear Sir or Madam, We would like to use NUCLEO-WL33CC2 to verify DMR RSSI reliable detection(compulsory requirement) and demodulation(optional requirement). We only need rx chain for scanning purpose. As per ETSI TS 102 361-1, DMR TDMA frame has s...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.