STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 299 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4116 Views
  • 0 replies
  • 3 kudos

PREAMBLE PQI check not working on STM32WL33xx

Hi, I'm searching for the best  Rx sniff mode as suggested in AN6362: I'm able to use carrier sense (RSSI_THR, CS_F interrupt) and SQI (SQI_THR, SYNC_VALID_F interrupt) but PQI never works.The MCU is in WFI state, sequencer not used.I have changed th...

syn by Associate II
  • 379 Views
  • 8 replies
  • 2 kudos

RTC in STM32WBA65 after reboot

I have an STM32WBA data logging project loosely based on the BLE heart rate project. I sync the RTC via either a BLE message, or NTP from a serial modem. All good; works well and the RTC timestamp ticks along whilst the code is in stop2 sleep. The de...

SLevi.1 by Senior
  • 175 Views
  • 0 replies
  • 0 kudos

STM32WL33CC1 MRSUBG stop receiving

void HAL_MRSubG_IRQ_Callback(void) { uint32_t irq = __HAL_MRSUBG_GET_RFSEQ_IRQ_STATUS(); if (irq & MR_SUBG_GLOB_STATUS_RFSEQ_IRQ_STATUS_RX_OK_F) { last_rx = HAL_GetTick(); HAL_GPIO_WritePin(LD1_GPIO_Port, LD1_Pin, GPIO_PIN_SET); if (H...

Tobias3 by Associate II
  • 394 Views
  • 6 replies
  • 1 kudos

STM32WL5MOCH6 Frequency Range

Hello Everyone,I'm checking the STM32WL5MOCH6TR MCU of a custom board that i made a few years ago, and I don't understand something : - On the datasheet, it says that its frequency range supported is 864–928 MHz- When I open a CubeIDE project, I'm ab...

Screenshot 2026-05-15 at 12.10.34.png Screenshot 2026-05-15 at 12.11.36.png
yaxsomo by Associate III
  • 181 Views
  • 2 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.