STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

P-NUCLEO-LRWAN3 Connectivity Issue

I am currently encountering difficulties with my P-NUCLEO-LRWAN3 board. It is worth noting that the board used to work flawlessly; however, it has recently encountered connectivity problems. Despite meticulously following the recommended setup proced...

ABell.5 by Associate II
  • 1534 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55 - How to implement Zigbee OTA cluster

 Hello,I hope this message finds you well. I am currently managing over eight Zigbee devices connected to one Coordinator in a star topology fashion (8 or more End devices to one Coordinator). However, the manual procedure for flashing new firmware i...

Resolved! stm32wba series dma request mapping table

I found the DMA request mapping of the F4 series on ST's official website. With this form, I can configure DMA on zephyr. My problem is that I cannot find the DMA request mapping of STM32WBA52CG. Can you provide me with one? Thank you.The device tree...

mteaching_1-1704244614689.png
mteaching by Associate III
  • 2983 Views
  • 2 replies
  • 1 kudos

ADS1219 not responding to I2C

ADS1219 Data SheetHello, I am attempting to communicate with TI's ADS1219 via I2C from a STM32WL55JCI, I know the I2C works becuase I can use the same line to write/read from a FRAM chip. Unfortunately, the ADS1219 communication always results in a H...

sgtaylor by Associate
  • 2761 Views
  • 4 replies
  • 1 kudos

Resolved! Nucleo-WL55JC Latency

Hello   I have two STM Nucleo-WL55JC2 boards. I have tried running the SubGHz_Phy_PingPong example and it works flawlessly.  When observed using TeraTerm, I am only able to see the RSSI and the SNR values.  I also need to observe the latency of this ...

Junk value (?) comes on serial port

Hi, we are using stm32wb55 board for wearable project. logs on serial port are fine when we flashed simple hello world program in loop. But when flashed the application menu developed by us we are seeing some junk value all the time. we are setting t...

STM32WB BLE SHCI_SUB_EVT_CODE_READY Event is NOT received

Hello, I am trying to figure out a root cause for a weird unexplainable error on STM32WB with BLE Stack. In our application, we have BLE stack fully functional, but every now and then, when we make a small change, like adding a debug line, APPE_SysUs...

Amogh by Associate III
  • 8917 Views
  • 17 replies
  • 0 kudos

Gfsk at 300kbps? - nucleo-wl55jc1

Hey,Im working with nucleo-wl55jc1 and I’m trying to work with 300kbps rate.I’ve read in the RM0453 reference manual that it is possible, but as I know the gfsk parameters doesn’t allow this rate.Can someone recommand gfsk parameters that work will w...

Gyuki by Associate
  • 934 Views
  • 0 replies
  • 0 kudos

BLE heart Rate data

this is the example of BLE heart rate ,its working  and showing data on ST BLE Sensor app.The data that is taken in the program is raw .i want to print data of ADC channel .how i can assign the ADC channel data to the app or how i can replace the ran...

RanjeetSingh_0-1692683763422.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.