NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I am using two NUCLEO WB15CC boards to make the BLE p2pcentral and BLE p2pServer work as said in the ReadMe of the these examples. But I always run into the same error on the client side. I am using the latest firmware on both sides. From the deb...
Hello, It is not clear to me if I can set stm32wb55 to advertise for connection (e.g., fast, slow) during sleep mode.In case a client connects to me, will I get a connection event that will wake CPU1?What are the sleep modes( power consumptions) of ...
What is the maximum Link Range in the SPSGRF running 868MHz in stm32 B-L475E-IOT01A2 Board ?
I want to know if the STM32WB series can operate normally with a main frequency of 100 kHz in low-power-run mode, including the RF part?
Hi,It's first time using st product to me.according to that's UM, i thought that connect CN11 to PC it work debugging.but it wasn't and showed warning message "No ST-LINK detected! Please connect ST-LINK and restart the debug session"ST-LINK isn't in...
I have just sent a notification to the client, but noticed , I did not get a notification confirmation event back.This event :(ACI_GATT_SERVER_CONFIRMATION_VSEVT_CODE) Since then, I cannot send any more notifications on the characteristic. Why is th...
Hi,currently, I am using an NX2016SA (as recommended by ST) to generate the HSE (32 MHz) for an STM32WB55RGV6 microcontroller.I did not calibrate it, but so far everything works and I have a BLE range of up to 25 meters.Now I am planning to getting m...
Hi all,I read this advertising in the datasheet:<<The SMPS needs a clock to be functional. If for any reason this clock stops, the device maybe destroyed.[...]Danger: Before enabling the SMPS, the SMPS clock detection must be enabled in the sub-GHz r...
I have a zigbee 3 client working on channel 11 . But It was developed by some other person who was not in touch anymore .. the issue is I need to develop a project that only read a temperature data and frequency value and send those 2 values over zig...
Hello,I am trying to comunicate the STM32U5 of the board with the STM32WB module, as I need a star network (1 client with 5 servers), I could also use a mesh. To comunicate different nodes. I am having trouble with it, as I just send basic "AT+BLE_RS...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.