NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I'm trying to flash \STM32Cube_FW_WB_V1.18.0\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB1x\stm32wb1x_BLE_Stack_full_fw.bin at address 0x08021000 with SMTCubProgrammer version 2.14.0I think that it is unsuccessful, and the application BL2_p...
I'm thinking of adding NVM functionality to Zigbee_custom_ls_Client_Router with p-nucleo-WB55. You may be able to receive it, but it will take too long. Please let me know if there is a possible cause.
Hi I am creating my own Zigbee sensor, where i have add support for it in Zigbee2MQTT, however I am not sure on how the set the STM32WB up to automatic report its measured temperature values up?I can select the endpoint, cluster, attributes i want to...
Though, I was able to run the point-to-point communication using the SubG_Phy ping-pong example using the STM32CubeIDE programmer with the STM32WL55JC1 board. However, if I just enable a GPIO port (making any minor changes in the configuration) to t...
Hi,I´m trying to port the example from above to my custom sensor board and use ZigBee2MQTT together with this board. You can find the code in the attachments.The board connects via ZigBee, but can not report the config[M4 APPLICATION] ZbStartup Callb...
I'm using a micro stm32wl55 (RAK3172). I try to shut it down using shutdown mode. By turning it off without ever using the PWR_SUBGHZSPICR command, the micro turns on and off regularly with the expected consumption. However, if I activate the PWR_SU...
Hi,i am working on stm32wb55 nucleo board.I want to read data form one location of internal flash e.g 0x08047000 and write into the other location e.g 0x08007000.i found there is HAL_FLASH_Program API available to write data into internal flash but i...
Hi, I'm currently developing for the STM32WB15CC. During code generation with CubxMX, Under the "BLE Applications and Services -> Server Mode", the option for "Custom Template" is missing when FreeRTOS(CMSIS_V2) is enabled. This option is present whe...
Whenever I plug my Nucleo WB55 into my PC via USB, a Drive opens with some basic info about the Board. While this may be helpful at the beginning I don't want that this opens up everytime I plug it in. Is there a way to disable this behaviour in the ...
Hello everyone. I started developing a zigbee zigbee application on a custom PCB, and since I don't need that much space I used the STM32WB55CC MCU. Everything went great until I had all components planted and wanted to update the zigbee stack when I...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.