STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How To get GPIO Input data in STM32F103

Hi, I want to make I2C By GPIO I/O Ports Using STM32F103RBT6 64 Pins.run my source code result is above figure.When I2C Input Read time, It Can’t read data how can I get input data?    Start_Setup_Time(); // b7 ~ b1 Addr + bo_wr + ack Setup_Addr(0x...

image.png

STM32F429IGT7 has a very serious problem

I found a very serious problem while using BOR, which caused my program to be erased innocently.At least 0x0800 0000-0x081f ffff is like this,This is the result obtained by jlinkI need to use the BOR function when I power on, originally this function...

SSss by Associate
  • 1913 Views
  • 3 replies
  • 0 kudos

Identifying STM32F429 Revision - New package marking?

Hello, i ordered a STM32F429ZGT6.Now i try to identify the revision of the chip i got.The marking on the package seems to have changed - there is no ARM Logo anymore.And where the revison was printed in the past there is now a QR-Code.Is 340 the date...

sk-st by Associate III
  • 3261 Views
  • 2 replies
  • 1 kudos

STM32F334 ADC Jumps

Hello, I am using a STM32F334 for a project where I am reading several analog channels, specifically connected to thermistors. I am using DMA to read the analog channels and also sending this data out on UART via DMA.  I am seeing some weird jumps in...

jls by Associate II
  • 9493 Views
  • 8 replies
  • 1 kudos

Resolved! Restart One Shot ADC + DMA

Hi,I have an STM32H747IGT6 that I wish to:Continuously sample 4096 ADC samplesTransfer each sample from the peripheral to memory using DMATrigger an interrupt at the end of the conversionsAfter the CPU operates on the stored data, restart the process...

slc2015 by Associate II
  • 3613 Views
  • 3 replies
  • 0 kudos

Sequence of 4 measurements using ADC1

I was unable to configure ADC1 to measure a "4 channel sequence" and then generate an interrupt.I am using the injected result registers to read the values in the ISR.Adc_Value[0]= ADC1->JDR1;Adc_Value[1]= ADC1->JDR2;Adc_Value[2]= ADC1->JDR3;Adc_Valu...

bolurian by Associate II
  • 5807 Views
  • 11 replies
  • 0 kudos

Resolved! STM32H725 Vcap pins

Hello,I would like to know whether I understood the application note about the Vcap pins correctly. If there are 3 Vcap pins on the package, then 2 capacitors should be placed and one has to be connected to another. I'm not sure about this connection...

1000003688.png
fing by Associate III
  • 7931 Views
  • 8 replies
  • 7 kudos

STM32F429 Automatically Enables Write Protection

Hello guys,In some of the products we developed with STM32F429, we received the write-protected error I mentioned in the image. I know how to turn off write protection, but I can't figure out how it activates independently. However, there are also ma...

abdullahcavuss_0-1705405905781.jpeg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.