STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! KSZ8863RLL (dual PHY) - datasheet typo/error?

Heyho,first of all, I know this is a Microchip product, but their forum is rather dead.And I have seen some people here using the KSZ8863RLL. So please bear with me... I'm currently working on a big and complex PCB including the "dual PHY" KSZ8863RLL...

LCE_1-1701932684775.png
LCE by Principal II
  • 1632 Views
  • 1 replies
  • 1 kudos

STM32H7 periodical TIM triggered SPI transfer w/o DMA?

On a STM32H745ZI-Q - Board I want to create periodical 4-byte SPI transfers  triggered by a timer. So far I got this working the following way:TIM triggers DMADMA initiates the SPI transfer.However, the SPI transfer timing (CS low) has a high jitter ...

MSZB by Associate II
  • 12192 Views
  • 28 replies
  • 3 kudos

Can't upload the firmware F405

HI all, I am building a system to control my battery charger.When I power up the system from the DC power supply it work perfectly.But when I power up this with AC power supply it gives below error. What can be the possible error?

Supun_C_0-1705375752436.png
Supun_C by Associate
  • 1322 Views
  • 1 replies
  • 0 kudos

Resolved! Having Problem with FP-AI-Vision_V3.1.0 counting people

Hello Everyone!I'm facing a problem with all the examples on this package FP-AI-Vision and my LCD only displays noises. I have the board STM32H747I-Disco model MB1248-H747I-D03 and the display MB1166-A09. I realized that in this package doesn't has t...

brunamark_0-1705356533647.png
brunamark by Associate III
  • 1556 Views
  • 1 replies
  • 0 kudos

STM32F407 write protected on chip

Hi folks, i have an STM32F407 discovery board. when i measure the voltage across the gpio pins it becomes write protected. after i dumped many codes but no use. i had attached the screenshot with the error code that it's display. i tried to put jum...

0690X000006C6OVQA0.png 0690X000006C6OQQA0.png
Ark1 by Associate II
  • 2763 Views
  • 5 replies
  • 0 kudos

I2C problem in reading VCNL 4040 proximity sensor

Hi,I got the VCNL4040 Proximity sensor breakout board. I tried this board with Arduino Uno example solution and works very well.Now, I am trying to read this sensor with an STM32L0 series MCU. I see I am able to write to the sensor by turning ON and ...

ashah.16 by Associate II
  • 3614 Views
  • 2 replies
  • 0 kudos

Resolved! Can't reset the core

Hi,When attempting to connect to an STM32F030C8T6 MCU, ST-LINK Utility gives the following error message:"Can not connect to target!If you're trying to connect to an STM32W1xx device, please select Normal or HotPlug mode from Target->Settings menu.If...

JS8 by Senior
  • 4780 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.