STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F756VGH6 unpredictable basic timer

Hi,I am at the beginning of my STM32F756VGH6 register programming journey. I have already setup everything, and now I am at the led blink (using a logic analyzer for measuring the time intervals). I decided to make a simple blocking delay function ou...

Vilius by Associate III
  • 7315 Views
  • 14 replies
  • 1 kudos

DMA and SPI - TEIF error

Posted on June 15, 2015 at 12:57 Hello I am a beginner in using STM32 devices, so please tell me if I am doing something incredibly wrong here. I am trying to enable DMA for SPI on STM21F411RE but I keep getting TEIF error on the SPI3 ch...

tbnkr by Associate II
  • 2402 Views
  • 4 replies
  • 0 kudos

SDIO comprehensive course

Hello everyone, as port of my role I am looking form SDIO comprehensive course. Can be either online or not. If any of the members can give a recommendation on how to ramp up well on SDIO protocol / use cases / specs / etc. it will be of great help. ...

I have a problem with HAL LWIP that is very troubling

  When I was using Cube MX software to generate LWIP examples for STM32F107, using RAW mode was very normal. But once FREERTOS  lwip is selected through CUBEMX, basic PING communication cannot be achieved. I am wondering if there is anything to pay a...

King by Associate
  • 1390 Views
  • 1 replies
  • 2 kudos

what is port output speed in STM32

Hi.I'm looking for some answer which I can not find anywere.What is the time between instruction execution time consisting of writing '1' to GPIO->BSRR of any pin and port and real mcu pin state in case when HCLK is e.g. 72MHz and APB2 is 4,5MHz (APB...

sholojda by Associate III
  • 1791 Views
  • 2 replies
  • 1 kudos

How to detect if USART is connected to a console app ?

As i state in the title, what is the best way to detect a connection to a console app on a pc?I want to include a while loop in my program, that stalls the main program until the user establishes a connection and the program proccedes to the super lo...

Stm32f407 - Error "can't reset the core" with ST-Link.

Hello, I am using STM32f407IGT6 with Keil uvision and HAL library. When I try to connect the device with ST-Link and flash the software using the JTAG interface, I always see "can't reset the core" as the error.BOOT0 - Connected to GNDBOOT1 - Connect...

ajain20_0-1705490340060.png
ajain20 by Associate
  • 1142 Views
  • 0 replies
  • 0 kudos

Best way to transfer strings to STM32 with USART ?

Hello guys. I'm fairly new to stm and i've mostly worked on a pico.The thing is that i want to create a programm with the following function.The user sends a character and then a string from a python app on my pc. The first character is a pseudo hand...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.