2024-01-16 1:34 PM
Hello,
i ordered a STM32F429ZGT6.
Now i try to identify the revision of the chip i got.
The marking on the package seems to have changed - there is no ARM Logo anymore.
And where the revison was printed in the past there is now a QR-Code.
Is 340 the date code? That would mean probably 2023 week 40.
2024-01-16 2:07 PM
The die is rev '4' out of Fab in France, ST Crolles CR300
REV_ID 0x2003
Encapsulation and final test in Taiwan
Mouser has several of the PCN
The '5' die come of a Fab in Taiwan, TSMC Fab14, same design files, different local mask set
2024-01-16 10:39 PM
Thank you for this information!
So the 4 right to VQ is the stepping?
Is it still the 90nm process in Crolles?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.