STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

dfsdm in zephyr

Dear everyone Microphone is connected to stm32f412's dfsdm block Is there an example of dfsdm control on zephyr ?thanksBRMr.shim 

hongjo by Associate II
  • 1522 Views
  • 1 replies
  • 0 kudos

STM32F405 - ADC Result Not Reaching Full Scale

Hello, I'm using the STM32F405RGT6 to continuously read 4 ADC channels with 12-bit resolution. The problem is that the results the ADC is giving seemed non-linear, as you can see in the Excel file attached, where I tested it by injecting voltage from...

Screenshot 2024-03-19 113502.png Screenshot 2024-03-19 113519.png Screenshot 2024-03-19 113734.png
racmatos by Associate
  • 2449 Views
  • 2 replies
  • 1 kudos

Placing STM32L433 into standby

Hi  I am using the STM32L433 in a battery product and need long battery life. I am using standby mode as I need to preserve RAM and the RTC during standby. We are testing a new blank board and adding components one at a time and measuring the current...

SSmit13_0-1710862081773.png SSmit13_1-1710862257124.png

STM32H753 and RTC return wrong day

In my project I want to use RTC on STM32H753 chip. And when reading the date, I get the wrong data in the position of days. And I can't fix this problem. When I debug, the registers are set successfully. :face_with_rolling_eyes: Init function:     vo...

STM32H7 has a FMAC, can it be tweaked to implement FFT?

STM32H7 has a FMAC (Filter mathematical accelerator), and FFT also build on multiply-accumulation operations similar to the filters. So, can the FMAC be tweaked to implement FFT with minimum MCU intervention. ​And also FFT calculation with M7 core wi...

YDao.1 by Associate
  • 3111 Views
  • 1 replies
  • 1 kudos

Resolved! CAN frame monitoring problem in loopback mode

@mƎALLEm hello again,   So , i am facing a problem to display the frame i am supposed to send from CAN_Tx pin in loopback mode. I am using picoscope to display. Here is the function i wrote to configure the Header, and send the data: void CAN_send(...

Erwan03 by Associate III
  • 4857 Views
  • 6 replies
  • 3 kudos

Resolved! Issue with CAN in loopback mode

Hello, i am using f446re nucleo board and have been facing a problem for a while now. I need to establish a loopback CAN transmission and the debug mode allows me to find a bug in the CAN Start function: HAL_ERROR 0x1 returned everytime i attempt. he...

Erwan03 by Associate III
  • 4239 Views
  • 7 replies
  • 2 kudos

Resolved! A bit disappointed about the STM32H7R/S lines

Dear ST,I was pleased to hear about the new STM32H7R/S lines, especially with the new graphic acceleration features in the R-line.However, and perhaps I have missed something, but I have to admit I am also disappointed about the absence of large size...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.