Resolved! 'H7 infographics: SMPS in 'H725?
DS says otherwise - that SMPS is available in *all* packages for 'H725: To me it appears that it's the infographics which is wrong. Wasn't the footnote supposed to go into some other sub-family?JW
Ask questions, find answers, and share insights on STM32 products and their technical features.
DS says otherwise - that SMPS is available in *all* packages for 'H725: To me it appears that it's the infographics which is wrong. Wasn't the footnote supposed to go into some other sub-family?JW
Hello,I am not able to find the memory map for the processors stm32f777zitx.It tells to refer to product line reference manual what does that mean?I checked everywhere on the internet but could not find it.
STM32F103C8T6 enables SPI1, but does not use MISO pin (PA6), can this pin reuse other functions? For example, timer function.
Hi, I got a problem with the reception using USART7. I'm using it in the interrupt mode but the problem is that the data in the buffer is not coming well. I'm connecting STM32F407 board with the STM32F746 using UART. When the F7 transmits, there's no...
Hi,I'm using STM32U575I-EV and CubeMX.Please tell me about benefits using lpbam in CubeMX.I thought that if I properly set up the peripherals that support LPBAM on the "Pinout & Configuration" screen, I could do the same thing as LPBAM Scenario.When ...
Hello,We use STM32F765VGT6 in our product. The datasheet says 1MB of flash memory available but it looks like there is 2MB available for use 0x0800 0000 to 0x081F FFFF. Is this a documentation issue? Can we use the extra 1MB flash starting from 0x081...
Hi, I have problem to generate correct output waveforms with Altium SI tool using the IBIS model stm32f765_767_777_lqfp144.ibs. I'm trying to generate a clock output signal in PB3 configured as SPI1, no pulls, fast speed or high speed but the result...
I finally got my hands on a STLINK-V3SET. I'm eventually going to use it on a custom board we're spinning up but I thought I'd start with STM32CubeIDE and a Nucleo-H7A3ZI-Q. I've tried several configurations per the manuals and always get this erro...
I just was testing the bootloader, when it did not respond after writing the flash. Upon inspecting the memory, i found the last 2 bytes have not been written? (i guess the uC went to hard fault or something)It should not be this way?
Hello, I am having an issue with the STM32 GPIO. The problem is that immediately after supplying power to the chip, GPIOs such as PJ0, PJ1, PJ2, etc. are momentarily powered, behaving as if they were set as outputs.Below is the test sequence:1. I cr...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.