STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bootloader to Main Appilication - SRAM Cleaning

hi,how to clean SRAM before jumping to main application from bootloader .In the SD card boot loader code we use local , global  & static variable and what will happen to these variables during the transition from boot loader to main application .how ...

MMARI.1 by Senior II
  • 922 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H7B3I-DK - LCD init through .ioc file does not work

As I mentioned earlier I am trying to show red color on display screen this time using HAL_drivers. I attached a video on my one drive of me configuring a .ioc file and I builded it with 0 errors but when I flashed it to hardware, display module does...

richi by Associate III
  • 1808 Views
  • 2 replies
  • 0 kudos

Which code in SRAM4 for LPBAM?

Hello,In the example projects for LPBAM from ST, it is necessary to switch the RAM address to the SRAM region. This is because LPDMA has in Stop2-Mode only access to SRAM4.If I also want to use the RAM, which part of LPBAM (or maybe other parts) must...

JoachimO_0-1710411635664.png
JoachimO by Associate II
  • 1766 Views
  • 2 replies
  • 0 kudos

STM32F103C8T6 pin multiplexing problem

hello,STM32F103C8T6 enables SPI1, but does not use MISO pin (PA6), can this pin reuse other functions? For example, timer function.Also, the PWM output can be observed in the software simulation, but there is no PWM output in the actual test. Is ther...

112233 by Associate II
  • 1377 Views
  • 1 replies
  • 0 kudos

Cannot get CC1 on TIM15 to go low using CCMR1 register

Using a Nucleo-F072RB.  I am trying to get the output of CC1 to go low after the CPU does something.  Everything is working as expected except I cannot get the line to go low.  I have tried both variants of the CC1P bit and neither seems to work.  I ...

SWenn.1 by Senior III
  • 12068 Views
  • 19 replies
  • 0 kudos

PSRAM Issue with STM32L4R9 Discovery Kit

Hi,Currently I am working with STM32L4R9 Discovery kit. The connected PSRAM model with this board is IS66WV1M16EBLL-55BLI. Using HAL functions, I can only write and read up to 16 bit data (i.e. unsigned integer 8 bit (uint8_t) and uint16_t). Other da...

SSG by Associate II
  • 935 Views
  • 0 replies
  • 0 kudos

STM32F103RB I2C1 Busy Flag stays high when initializing

I finished my I2C peripheral drivers and I would like to test it with my bh1750 sensor but I am having an issue, when i initialize the I2C1 peripheral, everything is smooth but then I notice that the busy flag is always high and it does not go low, s...

jdsus by Associate
  • 1114 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F401RE SPI1 CLK signal wrong

I am trying to use the SPI example code, and I configured SPI1 on the NUCLEO-F401RE board in full Duplex work mode.I connected two NUCLEO-F401RE boards together by GND, CLK, MOSI, MISO,and CS(but I use NSS_Soft mode).Because there is no example code ...

RichKnight_2-1711392463499.png RichKnight_3-1711392496131.png RichKnight_4-1711393605675.png RichKnight_1-1711392426733.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.