STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32h743ii serie with QSPI memory W25Q256JV

Hello all  Hardwarestm32h743iitxflash : W25Q256JV sdRam: w9825g6kh lcd : 7 pouces no driver 24bit parrallel I have dev a stm32h743ii pcb with a 7 pouces 24 bit lcd . the basic debug work for the lcd and sdramWhere i am facing problem is on flash W25Q...

qspi1.png
KNaim.1 by Associate III
  • 373 Views
  • 1 replies
  • 0 kudos

Multiple ADC Channels reading same values

Hi I'm using STM32G0B0RET6, and im using ADC Channel 1,4,5,6,7,10,11,15, and 16 . and sequencer is set to not fully configurable because if set to fully configurable then i can't use Channel 15 and 16.So here for all ADC channels i'm getting same val...

FW1 by Associate
  • 386 Views
  • 2 replies
  • 0 kudos

Resolved! stm32f103 partially receive from canbus and don't send

hello, I have a can bus with 2 node (one STM32G0B1 with SN65HVD1050DR  transcriver and one esp8266 with MCP2515 module) that comunicate over canbus at 1Mbps.I am trying to add a third node, it is a blue pill STM32F103C8T6. The chip onboard looks genu...

steeve by Associate
  • 265 Views
  • 1 replies
  • 0 kudos

Resolved! Any benefits for N6 without AI accelerator

I'm currently looking at something like thisSTM32N657A0But they sell a non AI accelerator version STM32N655A0Is there any benefits to using the non AI version of the chip.  Other then saving a few dollars on the chip? 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.