STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750 and USB3300-EZK has stopped working

I designed a board that uses a STM32H750 with a USB3300-EZK that has stopped communicating over USB. It's been having intermittent issues for the last day or so (sometimes I'd need to power cycle the board before it would show up, but then it would w...

sophie by Associate II
  • 890 Views
  • 10 replies
  • 2 kudos

Resolved! STM32H573 PB14

In our project I use STM32H573VIT6 LDO uC. We have a problem with the PB14 pin. We use 3 pins for LED control (PB10, PB13 and PB14, see photo). The problem with the PB14 is that the LED lights up dimly without code initialization. If PB14 is initiali...

gaso111 by Associate II
  • 15655 Views
  • 27 replies
  • 11 kudos

800 x 800 Display with STM32U5G9VJT6Q - possible?

Hi,we are trying to get a 800x800 display to work with the STM32U5G9VJT6Q, using either RGB888 or RGB565 in Video Mode (Burst).According to what we read it is definitely possible. Did we miss something?Could someone please confirm that is definitely ...

Ricko by Senior III
  • 8167 Views
  • 32 replies
  • 16 kudos

Resolved! STM32 ADC VREFINT / TEMP reads maximal value 4095

Hi,I’m trying to read internal temperature sensor on ADC1, but the ADC result is always 4095.I use STM32L471, and I know that the problem is not HW related, when I run a different bin it reads the temp ok.Tried to read VREFINT, raw value is also 4095...

Screenshot 2026-01-20 152910.png Screenshot 2026-01-20 153102.png Screenshot 2026-01-20 155308.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.