2026-01-25 1:17 AM
STM32f103
In the design guide it recommends to have something switching between vcc and gnd with 10kOhm series resistor, and i need my design to be grounded by default so i may not solder the header even, is it okay if i left the design like fig 1 instead of fig 2, and would it cause issues if i needed to pull it high?
2026-01-25 2:53 AM - edited 2026-01-25 2:54 AM
No issue. You may pull it down with anything up to 100k and provide some contacts for connecting it to Vdd for bootloader activation.
You may short BOOT0 to ground directly with a PCB trace if you don't need to invoke the bootloader via hardware.
2026-01-25 2:59 AM
The pull-up resistor has the advantage of allowing you to set the pin in question to a different level directly at the pin without creating a short-cut. If you are absolutely certain that you never want to switch the pin, you can also connect it directly to a fixed potential (e.g. GND for the BOOT pins) without a pull-up resistor. You can also omit the pull-up resistor if you use a switch/jumper.
Regards
/Peter
2026-01-25 5:46 AM
To minimise board space, I've always just used a single pull down resistor (no series resistor) with a test point/contact (close to the micro) I can use to pull Boot0 high if required. I think it is a safer design to always have a pull down resistor. I personally would never connect Boot0 directly to ground, sometimes you need to pull Boot0 high to revive a stuck chip.
2026-01-25 6:07 AM
If you don't reassign the SWD pins, and that's how you program, there's little need to be able to pull BOOT0 high.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.