2026-01-23 7:51 PM
I am using the debugging mode in STM32CubeIDE, and the compilation result shows that there is insufficient RAM.
27_Touch_Appli.elf section `.bss' will not fit in region `RAM'
region `RAM' overflowed by 94904 bytes
2026-01-23 10:23 PM
Assume you have a variable declared like:
some_type myvariable;then you can force the linker to place it in a spefic section like this:
some_type myvariable __attribute__ ((section (".anothersection")));The name of the section must correspond with the desired section in the ld file.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.