2025-10-11 6:32 PM - edited 2025-10-11 8:44 PM
Hi all - I am building an isolated power converter using a three phase forward converter topology. Each phase has a half bridge driving a transformer primary w.r.t. Vin/2 (split Vin). The transformer has a mid-tap secondary, rectified effectively acting like a buck regulator at 2x the primary frequency. I am using the HRTIM hardware to drive this.
So far it works great - I have my three phases A/B/C programmed like so (each has high-side 1, low-side 2):
A resets on master update, A1 set on A update, reset on A cmp1, A2 set on A cmp2, reset on A cmp3.
B resets on master cmp1, B1 set on master cmp1, reset on B cmp1, B2 set on B cmp2, reset on B cmp3.
C resets on master cmp2, C1 set on master cmp2, reset on C cmp1, C2 set on C cmp2, reset on C cmp3.
The master cmp1 and cmp2 are set at phase angles 60, 120. The maset compares and all three cmp2 are fixed, while the cmp1 and cmp3 are all set by the feedback code. Works perfectly.
For continuous mode, however, we can't run in voltage mode as there is no balancing of the phases, so we have to run in peak current mode. I have CTs on each primary, rectified, feeding to comparator inputs on the CPU. I have modified all the programming for the resets to reset EITHER on the above cmp1 or cmp3, or on an eevN mapped to the appropriate comparator output. The -IN for each of the three comparators maps to DAC1 ch1. I have set the DAC_MCR to 0x11 to connect only to internal peripherals, not external pin. I have enabled the comparators with no blanking, no hysteresis, non-inv.
I know the internal connections are working, because lowering the DAC value while running does cause early commutation, but it appears to latch on. Raising the DAC value does not restore simple duty cycle control. Also, it appears that using a single comparator on circuit A for reset of A1 and A2 seems to apply asymmetrically, as if it is latching on and not letting A2 fire.
Question 1: Did I do something *** here, attempting to use a single rectified CT primary current signal to a single comparator for both A1 and A2 commutation? I would think this is pretty standard.....
Question 2: Is there some setting I am missing to unlatch/reset the reset sensitivity to the comparator? I suspect that I am missing some subtlety in the EExFLTR settings regarding windowing and latching. I am setting EEFxR1 latch bits in the sample code below, but have tried without with no apparent difference.
Question 3: The eev1-eev5 appear to act differently than eev6-eev10. The former allow for "fast" mode, while the latter allow for digital filtering. Right now I am using the former, but now I see in fine print that when using external events for reset, it is edge sensitive even if set level sensitive, and fast mode not available....? Should I be using eev6-10 with digital filtering?
Below is my init code for the HRTIM. (All hard coded in gnu assy, not using Cube). (write is a simple macro using R0 & R1, self-explanatory. pause is a routine using TIM6 for various housekeeping delays.) For now I am focusing on channel A only -- I have good gate pulses for all six FETs, but right now I have FETs and transformer populated only for channel A to verify function of Ipk limiting.
Any help is appreciated. - Jeff Casey
write HRTIM_DLLCR,1 // start the calibration by setting CAL bit
write TIM6_ARR,99999
bl pause // wait 100 ms for DLL to stabilize
write HRTIM_DLLCR,1<<1 // set CALEN on for regular re-calibrations
write HRTIM_MCR, 0x2800000A // MREPU on, PREEN on, timers not yet enabled, no sync, CONT on, CKPSC=010 (*8)
write HRTIM_MCNTR,0 // master counter
write HRTIM_TIMACR,0x0802000A // PREEN on, CKPSC=010, continuous, TxREPU
write HRTIM_TIMBCR,0x0802000A // same
write HRTIM_TIMCCR,0x0802000A // same
write HRTIM_CNTAR,0
write HRTIM_CNTBR,0
write HRTIM_CNTCR,0
write HRTIM_MPER, 37499 // ARR sets main period. 1.2 GHz/32 kHz t=0 phA, on A1
write HRTIM_MCMP1R, 6249 // phase=60 deg t=0 phB, on B1
write HRTIM_MCMP2R,12499 // phase=120 deg t=0 phC, on C1
write HRTIM_CMP1AR,7000 // feedback adjust from 30-18720 reset phA, off A1
write HRTIM_CMP1BR,7000 // same reset phB, off B1
write HRTIM_CMP1CR,7000 // same reset phC, off C1
write HRTIM_CMP2AR,18749 // 50% point, fixed on A2
write HRTIM_CMP2BR,18749 // same on B2
write HRTIM_CMP2CR,18749 // same on C2
write HRTIM_CMP3AR,25750 // feedback adjust from (30-18720)+18750 off A2
write HRTIM_CMP3BR,25750 // same off B2
write HRTIM_CMP3CR,25750 // same off C2
write HRTIM_RSTAR, 1<<4 // A resets on MSTPER (Master timer period)
write HRTIM_SETA1R,1<<31 // bit 31 = A1 set on A update
write HRTIM_RSTA1R,0x01000008 // bit3=A1 rst on A cmp1, bit24 rst eev4=COMP1.out
write HRTIM_SETA2R,1<<4 // bit 4 = A2 set on A cmp2
write HRTIM_RSTA2R,0x01000020 // bit5=A2 rst on A cmp3, bit24 rst eev4=COMP1 out
write HRTIM_EEFAR1,1<<18 // latch bit for eev4
write HRTIM_RSTBR, 1<<5 // B resets on MSTCMP1 (Master timer compare 1)
write HRTIM_SETB1R,1<<8 // bit 8 = B1 set on M cmp1
write HRTIM_RSTB1R,0x02000008 // bit3=B1 rst on B cmp1, bit25 rst eev5=COMP3 out
write HRTIM_SETB2R,1<<4 // bit 4 = B2 set on B cmp2
write HRTIM_RSTB2R,0x02000020 // bit5=B2 rst on B cmp3, bit25 rst eev5=COMP3 out
write HRTIM_EEFBR1,1<<24 // latch bit for eev5
write HRTIM_RSTCR, 1<<6 // C resets on MSTCMP2 (Master timer compare 2)
write HRTIM_SETC1R,1<<9 // bit 9 = C1 set on M cmp2
write HRTIM_RSTC1R,0x00400008 // bit3=C1 rst on C cmp1, bit22 rst eev2=COMP4.out
write HRTIM_SETC2R,1<<4 // bit 4 = C2 set on C cmp2
write HRTIM_RSTC2R,0x00400020 // bit5=C2 rst on C cmp3, bit 22 rst eev2=COMP4.out
write HRTIM_EEFCR1,1<<6 // latch bit for eev2
write HRTIM_EECR1,0x29A40A40 // map comparators to HRTIM, fast, edge triggered
write HRTIM_OUTAR,0x00200020 // fault=inact, idle=inact, pol-acthi, both A1 & A2
write HRTIM_OUTBR,0x00200020 // same
write HRTIM_OUTBR,0x00200020 // same
UPDATE - further experimentation has this working. on channel A, I switched from source2 of eev4 to source3 of eev6 (both COMP1), and set the filter bits to 0011 (Fhrtim & 8 hits). At this point, the commutation appears symmetrical for A1 and A2 when reduced by lowering the DAC. It also recovers back to duty cycle control if the DAC level is raised. It took a lot of experimenting, but now works as intended. Sorry for posting, but i'll leave it up in case anybody else has similar problems. - Jeff
Solved! Go to Solution.
2026-01-24 11:21 AM
As the issue has been solved according to the OP it will be marked as solution to make a visibility for other users.
2026-01-24 11:21 AM
As the issue has been solved according to the OP it will be marked as solution to make a visibility for other users.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.